Hello,
I am using IMX1050 EVKB board with MQXv5.
My BSP is setup to use PIT timer as _bsp_systimer (timer that call _time_notify_kernel())
I would like to use the systick timer (systick_devif) as source.
When a switch from PIT to Systick timer, i have quite strange issue :
Task that call _sched_yield(); are never active again.
for exemple :
while( lwgpio_get_value(&btn1) == LWGPIO_VALUE_LOW )
{
_sched_yield();
}
Here is #define for PIT and SYSTICK Timer :
#define BSP_ALARM_FREQUENCY (200)
#define BSP_ALARM_RESOLUTION (1000 / BSP_ALARM_FREQUENCY)
#if 1
#define BSP_SYSTIMER_DEV systick_devif
#define BSP_SYSTIMER_ID 0
#define BSP_SYSTIMER_SRC_CLK CM_CLOCK_SOURCE_CORE
#define BSP_SYSTIMER_ISR_PRIOR 2
#define BSP_TIMER_INTERRUPT_VECTOR INT_SysTick
#else
#define BSP_SYSTIMER_DEV pit_devif
#define BSP_SYSTIMER_ID HWTIMER_PIT(1,0)
#define BSP_SYSTIMER_SRC_CLK CM_CLOCK_SOURCE_PERCLK
#define BSP_SYSTIMER_ISR_PRIOR 2
#define BSP_TIMER_INTERRUPT_VECTOR INT_PIT
#endif
Hwtimer init code :
result = hwtimer_init(&_bsp_systimer, &BSP_SYSTIMER_DEV, BSP_SYSTIMER_ID, BSP_SYSTIMER_ISR_PRIOR);
if (MQX_OK != result)
{
return result;
}
result = hwtimer_set_freq(&_bsp_systimer, BSP_SYSTIMER_SRC_CLK, BSP_ALARM_FREQUENCY);
if (MQX_OK != result)
{
hwtimer_deinit(&_bsp_systimer);
return result;
}
result = hwtimer_callback_reg(&_bsp_systimer,(HWTIMER_CALLBACK_FPTR)_bsp_systimer_callback, NULL);
if (MQX_OK != result)
{
hwtimer_deinit(&_bsp_systimer);
return result;
}
result = hwtimer_start(&_bsp_systimer);
if (MQX_OK != result)
{
hwtimer_deinit(&_bsp_systimer);
return result;
}
_time_set_hw_reference(CLOCK_GetPllFreq(kCLOCK_PllArm) / BSP_ALARM_FREQUENCY);
_time_set_ticks_per_sec(BSP_ALARM_FREQUENCY);
_time_set_hwticks_per_tick(hwtimer_get_modulo(&_bsp_systimer));
_time_set_hwtick_function(_bsp_get_hwticks, (void *)NULL);
I have check that _bsp_systimer_callback() is called properly by the hwtimer, and verify the period using a scope:
extern LWGPIO_STRUCT led1;
void _bsp_systimer_callback(void *dummy)
{
lwgpio_toggle_value(&led1);
_time_notify_kernel();
}
I both case, i get 100hz witch is what i expect (BSP_ALARM_FREQUENCY (200))
I have only one task runing (main_task) , the startup task is stop by _task_block();
const TASK_TEMPLATE_STRUCT MQX_template_list[] =
{
{ 1, Startup_task, 1500, 8, "hello", MQX_AUTO_START_TASK, 0, 0 },
{ 2, main_task, 1500, 8, "Bp", MQX_AUTO_START_TASK, 0, 0 },
{ 0 }
};
When the main task yield, it never become active again (with pit timer as systick source it works well)
what did i miss ?