rs2101 and access point "transmit beamforming"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

rs2101 and access point "transmit beamforming"

1,106件の閲覧回数
Jarpba
Contributor II

Beamforming - Wikipedia, the free encyclopedia

It seems RedPine wireless module rs2101 is not working correctly when transmit beamforming is enabled in wifi access point.

This issue appeared with HP ProCurve MSM460 access point. Packets seem to be received very unreliable. Pinging the client shows that 2/3 of packets are lost on average. When beamforming is disabled, everything works fine.

According to HP's help:

Beamforming only works with wireless clients that are configured to support it.

--> So, does this mean that rs2101 reports it does support it and that's why access point uses beamforming for this client?

--> Can support for beamforming be disabled in code?

--> Does someone know, if there are options in rtcs or redpine driver to make the module work with beamforming?

Thanks!

ラベル(1)
1 返信

932件の閲覧回数
Tarun_redpine
Contributor III

Hello Jari Vanhakyla

RS2101 doesn't have beamforming support in both TX and Rx direction. Is it possible to send the sniffer log of the same?

0 件の賞賛
返信