Hello ,
I thought it did something very simple but alas perhaps I lost my head and so any help is appreciated! (code warrior 10_3 and mqx4_0 kinetis platform)
I just added one more entry to cgi_link_tbl and get and I get a "too many initializers error"?
In cgi_index.c I added to the table
const HTTPD_CGI_LINK_STRUCT cgi_lnk_tbl[] = {
...
...
{ "led_form_currentvalues", cgi_led_form_currentvalues},
{ 0, 0 } // DO NOT REMOVE - last item - end of table
};
Then I defined the functiuon:
_mqx_int cgi_led_form_currentvalues(HTTPD_SESSION_STRUCT *session)
{
if (Operations.Platform=='c' )
{
CGI_SEND_STR("<font color=\"blue\">compact shelf</font>");
}
else if (Operations.Platform=='m' )
{
CGI_SEND_STR("<font color=\"blue\">min-shelf</font>");
}
else
{
CGI_SEND_STR("<font color=\"blue\">unknown</font>");
}
return session->request.content_len;
}
I declared in cgi.h
_mqx_int cgi_led_form_currentvalues(HTTPD_SESSION_STRUCT *session);
The tfs_data.c was regenerated ith said function.
This was a formula I followed multiple times and no problem, but this time.....?
Any help would be appreciated.
EDIT:
Please use C++ highlight for code (last icon (>>)) Message was edited by: Martin Kojtal
解決済! 解決策の投稿を見る。
Hello joe krell,
I edited your message to highlight a code. I suggest using the advanced editor.
Have you checked the declaration for HTTPD_CGI_LINK_STRUCT ?
typedef struct httpd_fn_link_struct {
char fn_name[HTTPDCFG_MAX_SCRIPT_LN + 1];
FN_CALLBACK callback;
} HTTPD_FN_LINK_STRUCT;
HTTPDCFG_MAX_SCRIPT_LN is set to 16 by default, "led_form_currentvalues" contains more than the limit which is defined. That explains the error shown.
Regards,
0xc0170
Hello joe krell,
I edited your message to highlight a code. I suggest using the advanced editor.
Have you checked the declaration for HTTPD_CGI_LINK_STRUCT ?
typedef struct httpd_fn_link_struct {
char fn_name[HTTPDCFG_MAX_SCRIPT_LN + 1];
FN_CALLBACK callback;
} HTTPD_FN_LINK_STRUCT;
HTTPDCFG_MAX_SCRIPT_LN is set to 16 by default, "led_form_currentvalues" contains more than the limit which is defined. That explains the error shown.
Regards,
0xc0170
Hello Martin
Thank you very much! That was exactly the problem!
Regards
Joe