i develop application in code warrior 10.2 based on mqx4.0 for serial port.for none parity and its working fine.
what when i try same application for odd parity its not working.....
here i attach application
its very argent
any one can help??????
Original Attachment has been moved to: test_serialzip.zip
Hi
I have tried to test odd parity on K70 (no pxn board on my side).
I enabled uart2 with even parity , using IO_IOCTL_SERIAL_SET_PARITY , then I checked the parity type using IO_IOCTL_SERIAL_GET_PARITY, the result is right.
I checked the register value of uart2, it is even parity enabled. it means MQX can configure the right value to register.
I think you can check if you can get the right register value on your board.
You also can refer to the following link.
https://community.freescale.com/message/64746#64746
Have a nice day,
Daniel