new project on CW10.1 with MQX3.7 for TWRK60N512 - errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

new project on CW10.1 with MQX3.7 for TWRK60N512 - errors

Jump to solution
2,388 Views
avoicu
Contributor I

I just trying to create a new RTCS project inin CW10.1 & MQX3.7 for TWRK60N512 and I'm getting some errors and warnings when compiling.

 

CW10.1 has all the current updates installed.

 

Here are the steps I'm following to create the new project:

- New MQX 3.7 Project:

- TWRK60N512 Board

- Add RTCS Support

- Basic Application

- RTCS Options - Static IP

- Connection: P&E Open Source JTAG

 

When compiling for RAM - I getting the errors&warings from the attached figure, if I compile for FLASH (Debug or Release) I'm getting only the warnings but the project is not working as it should be.

 

Any idea what is going wrong? Any help is appreciated.

 

adis

 

PS When I did same thing with CW10.0 and MQX3.6.2 for a CF tower board everything worked fine

 

 

1 Solution
1,916 Views
petr_uhlir
NXP Employee
NXP Employee

Adis,

there is not enough RAM to run RTCS application on K60. You have to use FLASH target, it works OK.

I have tested it with console remapped to TWR-SER board (Default is K60 USB-SER)

 

// change in user_config.h and recompile the BSP

#define BSPCFG_ENABLE_TTYD       1

#define BSP_DEFAULT_IO_CHANNEL                  "ttyd:"    /* TWR-SER   polled mode   */

#define BSP_DEFAULT_IO_CHANNEL_DEFINED

 

If you connect serial terminal to UART you should see

 

Waiting for ethernet cable plug in ... Cable connected
IP Address      : 192.168.1.200
Subnet Address  : 255.255.255.0
Gateway Address : 0.0.0.0
DNS Address     : 0.0.0.0

 

Ping from PC connected on the same network

 

Ethernet adapter Local Area Connection 4:
Connection-specific DNS Suffix  . :       

IP Address. . . . . . . . . . . . : 192.168.1.100       

Subnet Mask . . . . . . . . . . . : 255.255.255.0       

Default Gateway . . . . . . . . . :

 

D:\Profiles\r51423>ping 192.168.1.200

 

Pinging 192.168.1.200 with 32 bytes of data:
Reply from 192.168.1.200: bytes=32 time=46ms TTL=64

Reply from 192.168.1.200: bytes=32 time=1ms TTL=64

Reply from 192.168.1.200: bytes=32 time=2ms TTL=64

Reply from 192.168.1.200: bytes=32 time<1ms TTL=64

 

Everything works OK. Can you please describe your issue in more details?

 

 

There is one error I have found in MQX Project Wizard.

When you create new project which uses USB HOST library, wizard does not copy usb_classes.h into project directory.

The following workaround can be used.

 

Copy "usb_classes.h" file from 

"{MQX 3.7 Install Directory}\tools\codewarrior_extensions\CW MCU v10.1\mqx_p2_repository\wizard_files\mqx\3.7\src\usb_classes.h" 

to 

"{New Project Directory}\Sources\usb_classes.h"

 

and rebuild project.

 

View solution in original post

3 Replies
1,917 Views
petr_uhlir
NXP Employee
NXP Employee

Adis,

there is not enough RAM to run RTCS application on K60. You have to use FLASH target, it works OK.

I have tested it with console remapped to TWR-SER board (Default is K60 USB-SER)

 

// change in user_config.h and recompile the BSP

#define BSPCFG_ENABLE_TTYD       1

#define BSP_DEFAULT_IO_CHANNEL                  "ttyd:"    /* TWR-SER   polled mode   */

#define BSP_DEFAULT_IO_CHANNEL_DEFINED

 

If you connect serial terminal to UART you should see

 

Waiting for ethernet cable plug in ... Cable connected
IP Address      : 192.168.1.200
Subnet Address  : 255.255.255.0
Gateway Address : 0.0.0.0
DNS Address     : 0.0.0.0

 

Ping from PC connected on the same network

 

Ethernet adapter Local Area Connection 4:
Connection-specific DNS Suffix  . :       

IP Address. . . . . . . . . . . . : 192.168.1.100       

Subnet Mask . . . . . . . . . . . : 255.255.255.0       

Default Gateway . . . . . . . . . :

 

D:\Profiles\r51423>ping 192.168.1.200

 

Pinging 192.168.1.200 with 32 bytes of data:
Reply from 192.168.1.200: bytes=32 time=46ms TTL=64

Reply from 192.168.1.200: bytes=32 time=1ms TTL=64

Reply from 192.168.1.200: bytes=32 time=2ms TTL=64

Reply from 192.168.1.200: bytes=32 time<1ms TTL=64

 

Everything works OK. Can you please describe your issue in more details?

 

 

There is one error I have found in MQX Project Wizard.

When you create new project which uses USB HOST library, wizard does not copy usb_classes.h into project directory.

The following workaround can be used.

 

Copy "usb_classes.h" file from 

"{MQX 3.7 Install Directory}\tools\codewarrior_extensions\CW MCU v10.1\mqx_p2_repository\wizard_files\mqx\3.7\src\usb_classes.h" 

to 

"{New Project Directory}\Sources\usb_classes.h"

 

and rebuild project.

 

1,916 Views
shane
Contributor I

+1

0 Kudos
Reply
1,916 Views
plasmaphase
Contributor I

I have exactly the same error.  I am using the K40X256 KwikStik board, and am just using the "Basic" project with no code changes at all.  I am interested in solution.

0 Kudos
Reply