nandflash example in mqx

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

nandflash example in mqx

1,254 次查看
ava
Contributor II

Hello everyone,

       I am using MQX4.1 CW10.6 & MK60FX512VLQ12 controller on our custom board.

I have tested nandflash demo example on TWRK60F120M & is working fine.Now I am trying it on my custom board & getting output as

MQX NAND Flash Example Application

==================================

NAND Flash device nandflash: opened

Obtaining NAND Flash organization data ...

ID:                      0x0

Physical page size:      2048 bytes

Spare area size:         64 bytes

Block size:              131072 bytes

Number of blocks:        2048

Width:                   16

Number of virtual pages: 524288

Virtual page size:       512 bytes

Block #1 is bad

Block #2 is bad

Block #3 is bad

Block #4 is bad

Block #5 is bad

Block #6 is bad

............

Block #2047 is bad

Size of the write buffer allocated in RAM: 16384 bytes

Erasing block #0 failed.

Writing data to 16 virtual pages of block #0 ... Done

Reading data back from 16 virtual pages of block #0 ... Failed

Comparing data ... Compare failed

I have done clock setting

SIM_CLKDIV4 &=  0x00FFFFFF; /* clear 8 most significant bits */

SIM_CLKDIV4 |=  SIM_CLKDIV4_NFCDIV(7);

as given in discussion -

Re: FFS on NANDFLASH of TWR-K70 (MQX 4.0.1)

this is also not working.What may be wrong in this.

Any solution?

Thanks for the help.

标记 (3)
0 项奖励
回复
2 回复数

942 次查看
soledad
NXP Employee
NXP Employee

Hi T tech;

It is necessary to check the hardware connections; does the custom board have the same hardware connection than the TWR-K60F120M?

We have non-MQX project for NAND Flash Controller(NFC). please use the KINETIS_120MHZ_SC sample code to evaluate nfc. This is in order to isolate the issue.

Please download the code from the link below:
https://www.freescale.com/webapp/sps/download/license.jsp?colCode=KINETIS_120MHZ_SC&appType=file2&lo...
see path ..\KINETIS_120MHZ_SC\KINETIS_120MHZ_SC\build\cw\nfc


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

942 次查看
ava
Contributor II

Hi Sol,

Thanks for the reply.

Hardware connection is same as TWRK60F120M.

Done some touch up to MK60FX512VLQ12 & now its working fine.

Thanks.

0 项奖励
回复