nandflash bad blocks

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

nandflash bad blocks

跳至解决方案
1,142 次查看
adt
Contributor III

Hi All,

        I have successfully tested nandflash using MQX4.1 & CW10.6 on TWRK60F120M board.

We have created our custom board same as TWRK60F120M board using MK60FX512VLQ150 controller.

For nandflash testing I used nand example from mqx without FFS but here I am getting ID as 0x0 and all blocks as bad.

I have tested 2 boards and for both boards getting the same output.

Thanks.

0 项奖励
回复
1 解答
1,004 次查看
adt
Contributor III

Added clock setting in _bsp_nandflash_io_init

SIM_CLKDIV4 &=  0x00FFFFFF;

SIM_CLKDIV4 |=  SIM_CLKDIV4_NFCDIV(7);

& now nandflash is working properly.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,005 次查看
adt
Contributor III

Added clock setting in _bsp_nandflash_io_init

SIM_CLKDIV4 &=  0x00FFFFFF;

SIM_CLKDIV4 |=  SIM_CLKDIV4_NFCDIV(7);

& now nandflash is working properly.

0 项奖励
回复