mqx based code working on some board and not on few

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mqx based code working on some board and not on few

964 Views
karanpatel
Contributor I

I develop one application using code worrior 10.2 and mqx rtos.one part of this application dose following things

-erase one part of flash

-programme it

i am using standard c90fl flash driver .

on many board this application work fine but on some bord its stuck when erase command used.all voltages on such board is ok and even i can programme it using debugger.what should be the problem????

i am using mpc5668g controller and same driver i am using in one previous application which is not based on mqx rtos and never face such problem.

0 Kudos
Reply
2 Replies

862 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please  let me know which mqx version are you using??

Regards

Sol

0 Kudos
Reply

862 Views
karanpatel
Contributor I

MQX_4_0 and using c90fl flash driver.and code got stuck when i call flash erase driver on some board and working on others.voltages are ok as i can programme same board with debugger and boot loader developed with out mqx

0 Kudos
Reply