I am still using TWR-K60N512 with MQX.
Datasheets says there are 10 power modes: run, wait, VLPR, VLPW, VLPS, LLS, VLLS3, VLLS2, and VLLS1
Some other datasheet also says there is a VLLS0
However, MQX just offers RUN, WAIT, STOP, VLPR, VLPW, VLPS, and LLS.
Are there VLLS3-2 modes ? Is there a VLLS0 mode ? How exactly can I configure and use them with MQX ?
That is really confusing...
My idea is that MCU is always in the lowest power consumption. When a timer (Low Power or RTC) interrupt or a button (LLWU) is pressed, interrupt routines are exectuted and MCU wakes up ( maybe at 2MHz or even lower). After executing some functions it goes back to the lowest power consumption.
I just need a timer and a pin interrupt.
Thanks in advance
Pasini