k60 mqx3.8 ulpi hs support with USB3300

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

k60 mqx3.8 ulpi hs support with USB3300

1,097 Views
kyles
Contributor I

hello,

Using a USB3300 trying to use ulpi hs mode,

MQX 3.8 that supports external ulpi hs?

If that support is apon the MQX need to upgrade?

The purpose is created using the USB3300 NAND flash and SD card as a mass storage device

NAND Flash and SD card both want to look in the window

In that setting, where you want to use an external ulpi?

Different questions

OTG is that the HOST, DEVICE both support?

When connected to a Windows USB3300 alone device name is what?

0 Kudos
5 Replies

560 Views
kyles
Contributor I

Hi Soledad,

Thank you for answer.

This series is k60fn120 be upgraded to MQX 4.2

It does not support?

Thank you...

0 Kudos

560 Views
soledad
NXP Employee
NXP Employee

Hi,

MQX 4.2 supports the K60 devices however MQX 4.2 contains two USB stacks.

New USB Unified stack is designed to replace the legacy USB stack in MQX RTOS, it has an OSA layer so that it can support different operating systems, like MQX RTOS, bare metal or other RTOS (like, FreeRTOS or μCos in KPSDK).

The New USB Unified stack (usb_v2) doesn't support the k60fn120 device. The legacy USB stack supports the K60 devices, however you can port the legacy USB stack to USB_v2, please find more information about the difference between old USB stack in MQX™ RTOS and new USB Unified stack and how to port the USB unified Stack to a new platform, in the docs attached.

Regards

Sol

0 Kudos

560 Views
soledad
NXP Employee
NXP Employee

Hi,

MQX 3.8 doesn't support USB OTG.

For ulpi hs please check the below thread:


Virtual Communication (COM) Demo - CDC device is necessary

I hope this helps, have a nice day!


Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

560 Views
kyles
Contributor I

Hello Soledad,

Thank you for answer.

What MQX version supported?

Thank you.

0 Kudos

560 Views
soledad
NXP Employee
NXP Employee

Hello,

MQX 4.2 contains a new Host and Device USB stack version 2 (same as in KSDK 1.2.0).

The new USB stack is available for following platforms : FRDM-K64F, FRDM-K22F, TWR-K21F120M, TWRK22F120M,

TWR-K64F120M, TWR-K65F180M, TWR-VF65GS10, SVF522R EVB.

and below are the new added features:

 Device:

  • Support multiple languages
  • Support multiple configuration descriptors
  • Composite Device support

 Host:

  • Support multiple configuration descriptors
  • Composite Device support
  • Unsupported device notification

 OTG:

  • Session Request Protocol (SRP)
  • Host Negotiation Protocol (HNP)

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos