Why is gstimxcommon.h in a gstream package instead of imx-gst1.0-plugins package?
I built gstreamer1.0-1.16.0 and now imx-gst1.0-plugin fails missing gstimxcommon.h
Somebody messed up putting gstimxcommon.h in old gstreamer code, vs putting it in imx-gst1.0-plugin.
Is there a newer version of imx-gst1.0-plugin available yet?
Terry
this is the latest version for 4.14.98 bsp
do you mean gstimxcommon.h instead of which file in the imx-gst1.0-plulgin? tell me the path, I send the imx-gst1.0-plugin source code to you:
https://source.codeaurora.org/external/imx/imx-gst1.0-plugin/tree/?h=MM_04.04.04_1811_L4.14.78_GA