iMX8 with tja1101

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMX8 with tja1101

2,519 Views
muhamed_emad-el
Contributor I

Im trying to write a Device Tree node for iMX8 ethernet (fec2) with TJA1101 (rmii mode) as the phy transceiver.

1- Is there anything missing with the nodes names and types in the device tree that will be looked for at linux kernel 4.14.98.

2- The tja1101 driver is supposed to be supported with the tja110x.c driver. is there any configuration that could be done to select tja1101 specifically.

I tried to include the tja110x.dtsi with my dts. And as an example of the device tree nodes...

--------------------------------------------------------EOF
&fec1 {
   status = "disabled";
};

fec2: ethernet@5b050000 {
   compatible = "fsl,imx8qm-fec";
   reg = <0x0 0x5b050000 0x0 0x10000>;
   interrupt-parent = <&wu>;


   interrupts = <GIC_SPI 262 IRQ_TYPE_LEVEL_HIGH>,
                        <GIC_SPI 260 IRQ_TYPE_LEVEL_HIGH>,
                        <GIC_SPI 261 IRQ_TYPE_LEVEL_HIGH>,
                        <GIC_SPI 263 IRQ_TYPE_LEVEL_HIGH>;
   

   clocks = <&clk IMX8QXP_ENET1_IPG_CLK>, <&clk IMX8QXP_ENET1_AHB_CLK>, <&clk IMX8QXP_ENET1_RGMII_TX_CLK>, <&clk IMX8QXP_ENET1_PTP_CLK>, <&clk IMX8QXP_ENET1_TX_CLK>;

   clock-names = "ipg", "ahb", "enet_clk_ref", "ptp", "enet_2x_txclk", "phy";
   

   assigned-clocks = <&clk IMX8QXP_ENET1_ROOT_DIV>, <&clk IMX8QXP_ENET1_REF_DIV>;
   assigned-clock-rates = <250000000>, <125000000>;
   fsl,num-tx-queues=<3>;
   fsl,num-rx-queues=<3>;
   fsl,wakeup_irq = <0>;   
   power-domains = <&pd_conn_enet1>;
   status = "disabled";
};

&fec2 {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_fec2>;
   phy-mode = "rgmii-txid";
   phy-handle = <&ethphy1>;
   phy-supply = <&reg_fec2_supply>;
   fsl,magic-packet;
   fsl,rgmii_rxc_dly;
   status = "disabled";
};

&fec2 {
   pinctrl-0 = <&pinctrl_fec2_rmii>;
   clocks = <&clk IMX8QXP_ENET1_IPG_CLK>,<&clk IMX8QXP_ENET1_AHB_CLK>,<&clk IMX8QXP_ENET1_REF_50MHZ_CLK>,<&clk IMX8QXP_ENET1_PTP_CLK>,<&clk IMX8QXP_ENET1_TX_CLK>;

   phy-mode = "rmii";
   phy-handle = <&ethphy2>;
   /delete-property/ phy-supply;

      mdio {
         #address-cells = <1>;
         #size-cells = <0>;

         ethphy2: ethernet-phy@2 {
         compatible = "ethernet-phy-ieee802.3-c22";
         reg = <2>;
         tja110x,refclk_in;
      };
   };
};


pinctrl_fec2_rmii: fec2rmiigrp {
   fsl,pins = <
      SC_P_ENET0_MDC_CONN_ENET1_MDC 0x06000020
      SC_P_ENET0_MDIO_CONN_ENET1_MDIO 0x06000020
      SC_P_ESAI0_FSR_CONN_ENET1_RCLK50M_OUT 0x06000020
      SC_P_SPDIF0_RX_CONN_ENET1_RGMII_RXD0 0x06000020
      SC_P_ESAI0_TX3_RX2_CONN_ENET1_RGMII_RXD1 0x06000020
      SC_P_ESAI0_TX2_RX3_CONN_ENET1_RMII_RX_ER 0x06000020
      SC_P_SPDIF0_TX_CONN_ENET1_RGMII_RX_CTL 0x06000020
      SC_P_ESAI0_TX4_RX1_CONN_ENET1_RGMII_TXD0 0x06000020
      SC_P_ESAI0_TX5_RX0_CONN_ENET1_RGMII_TXD1 0x06000020
      SC_P_ESAI0_SCKR_CONN_ENET1_RGMII_TX_CTL 0x06000020
   >;
};

--------------------------------------------------------EOF

while the output from the kernel was

"

[ 4.471375] fec 5b050000.ethernet: 5b050000.ethernet supply phy not found, using dummy regulator
[ 4.485249] fec 5b050000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
[ 4.495277] fec 5b050000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 7a:ae:db:cd:b2:0f
[ 4.538153] mdio_bus 5b050000.ethernet-1: MDIO device at address 2 is missing.
[ 4.549625] fec 5b050000.ethernet eth0: registered PHC device 0
[ 40.369287] fec 5b050000.ethernet eth0: Unable to connect to phy

"

Is there anything here is not right. 

0 Kudos
3 Replies

2,323 Views
igorpadykov
NXP Employee
NXP Employee

Hi Muhamed

dts example of  iMX8 ethernet (fec2) with TJA1101 can be found on

fsl-imx8qxp-enet2-tja1100.dtsi\freescale\dts\boot\arm64\arch - linux-imx - i.MX Linux kernel 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,323 Views
muhamed_emad-el
Contributor I

thats exactly what i followed, you can look at the last fec2 node i have. but still no good results like the output i wrote.

0 Kudos

2,323 Views
igorpadykov
NXP Employee
NXP Employee

please try to reproduce issue on NXP MEK reference board with

latest Demo Images from

i.MX Software | NXP 

Best regards
igor

0 Kudos