how to use the External SRAM in MQX base on K60F120

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to use the External SRAM in MQX base on K60F120

ソリューションへジャンプ
1,157件の閲覧回数
qinchenghu
Contributor I

in the K60F120,there has a SRAM,now the MQX  has add the configuration in _bsp_flexbus_setup(0) and _bsp_flexbus_mram_setup().but in the application program,how can i use the SRAM? for example,i want to define a big data array in the SRAM .

0 件の賞賛
返信
1 解決策
939件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi qin chenghu,

Please check the below threads and let me know if this helps,

Best Place to add external SRAM in MQX

Anybody added external SRAM to Kinetis K60 while using MQX.
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
940件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi qin chenghu,

Please check the below threads and let me know if this helps,

Best Place to add external SRAM in MQX

Anybody added external SRAM to Kinetis K60 while using MQX.
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
939件の閲覧回数
qinchenghu
Contributor I

thank you,i will try it.

0 件の賞賛
返信