how to use the External SRAM in MQX base on K60F120

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to use the External SRAM in MQX base on K60F120

Jump to solution
1,122 Views
qinchenghu
Contributor I

in the K60F120,there has a SRAM,now the MQX  has add the configuration in _bsp_flexbus_setup(0) and _bsp_flexbus_mram_setup().but in the application program,how can i use the SRAM? for example,i want to define a big data array in the SRAM .

0 Kudos
Reply
1 Solution
904 Views
soledad
NXP Employee
NXP Employee

Hi qin chenghu,

Please check the below threads and let me know if this helps,

Best Place to add external SRAM in MQX

Anybody added external SRAM to Kinetis K60 while using MQX.
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
905 Views
soledad
NXP Employee
NXP Employee

Hi qin chenghu,

Please check the below threads and let me know if this helps,

Best Place to add external SRAM in MQX

Anybody added external SRAM to Kinetis K60 while using MQX.
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
904 Views
qinchenghu
Contributor I

thank you,i will try it.

0 Kudos
Reply