how to set/change gateway setting or make it accept connection from different subnet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to set/change gateway setting or make it accept connection from different subnet

3,799 次查看
David_Wu
Contributor III

I noticed the gatewy settings in IP Config in RTCS menu in CW10.2

gateways

  network                         gateway

  0.0.0.0/0                       192.168.100.1

  192.168.1.102/32       192.168.1.102

 

My configuration is: DHCP enabled - got an IP 192.168.100.185, gateway 192.168.100.1, netmask 255.255.255.0.

I can connect 192.168.100.185  from 192.168.100.4 - same subnet - but I couldn't from 192.168.1.102

 

Anyone know if the gateway setting is correct in MQX RTCS and if not how to change it? (I know how to set the default gateway - I don't know how to change the extra gateway info above -). Why there is an extra routing entry?

 

what settings can make it accept a connection from a different subnet - timeout issue, routing issue, socket option issue , what ever to make it work?

 

thanks in advance,

 

David 

标签 (1)
标记 (1)
0 项奖励
回复
7 回复数

2,979 次查看
GottiLuca
Contributor IV

Dear David,

It's quite normal that you could not connect to another subnet .

In such cases you have two options :

- You can try to connect the two nodes directly ( i.e. : without using gateway ) increasing the  netmask from 255.255.255.0 to a larger one ( i.e. : 255.255.0.0 ). In such a case, you have to set this same netmask on the other node ( 192.168.1.102 ).

- if you don't wanna modify the netmask, you muast have a gateway ( 192.168.100.1 ) that routes the messages bidirectonally from the two subnets ( 192.168.100.x and 192.168.1.x ) . This is usually a functionality that requires a routers or , more appropriate ,a firewall .


0 项奖励
回复

2,979 次查看
David_Wu
Contributor III
updates:It seems there is no route back to the host that makes the connection. I got the error is:TCP: TCP_Send_IP_packet: errno 1510 on IP_send.If I change the netmask to accommodate two subnets then the TCP connection works. Further investigation indicates that it looks like MQX did not support ICMP redirect messages from gateway.

 

0 项奖励
回复

2,979 次查看
David_Wu
Contributor III

By changing the netmask is only a work around and not a fix - I'd like to know if the MQX team will find a solution?

0 项奖励
回复

2,979 次查看
butok
NXP Employee
NXP Employee

The communication between two nodes from different networks is done via a gateway.

Nodes can communicates directly (without gateway) only if they belong to the same network. It is defined by the netmask.

0 项奖励
回复

2,979 次查看
David_Wu
Contributor III

But when it comes to ICMP redirct, things changed. If the Default gateway tells the K60 to contact the end device directly then regardless the netmask, K60 should setup a ROUTING rule for it to reach.

Here is what I did as a work around (add a indirect routing rule):

in icmp.c for case ICMPTYPE_REDIRECT in ICMP_service() I add the detection for redirect for a host and call RTCSCMD_internal(parms, IPIF_gate_add_redirect_other) instead - IPIF_gate_add_redirect_other is the function I added in ipif_add.c (see below ) - note that I add two more parameters in IP_route_add_indirect(). Also in IP_route_test() I check for RTF_REDIRECT_HOST flag and return the correct info if match.

I might miss some source code - but you should get the idea.

-----------------

icmp.c

------------------

@@ -99,7 +99,7 @@

    _ip_address          source, dest;

    uint_32              error;

    uint_16              chksum;

-   uchar                type;

+   uchar                type, code;

    ICMP_cfg_ptr = RTCS_getcfg(ICMP);

@@ -109,6 +109,7 @@

    source = IP_source(pcb);

    dest   = IP_dest(pcb);

    type = ntohc(packet->TYPE);

+   code = ntohc(packet->CODE);

    /*

    ** Make sure that

@@ -170,6 +171,14 @@

             parms.network = origdest;

             parms.netmask = 0xFFFFFFFFL;

             parms.locmask = 0;

+#define ICMP_REDIRECT_FIX 1

+#if ICMP_REDIRECT_FIX //WMQ

+            parms.ihandle = pcb->IFSRC;

+            if(code == ICMPCODE_RD_HOST){

+               parms.address = dest;

+               RTCSCMD_internal(parms, IPIF_gate_add_redirect_other);

+            } else

+#endif

             RTCSCMD_internal(parms, IPIF_gate_add_redirect);

          } else {

             IF_ICMP_STATS_ENABLED(ICMP_cfg_ptr->STATS.COMMON.ST_RX_DISCARDED++);

---------------------------------------

rtcs/source/tcpip/ipif_add.c

-----------------------------------------    

+/* for ICMP redirect when gateway is the destination */

+void IPIF_gate_add_redirect_other

+   (

+      IPIF_PARM_PTR  parms

+   )

+{ /* Body */

+

+#if RTCSCFG_ENABLE_IP4

+

+   _ip_address          netmask = parms->netmask;

+   uint_32              error;

+

+   /*

+   ** Make sure the netmask is valid.  We use the fact that

+   ** (x & x+1) == 0  <=>  x = 2^n-1.

+   */

+   if (~netmask & (~netmask + 1)) {

+      RTCSCMD_complete(parms, RTCSERR_IP_BIND_MASK);

+      return;

+   } /* Endif */

+

+   /* Start CR 1133 */

+   //error = IP_route_add_direct(parms->address, parms->netmask, (IP_IF_PTR)parms->ihandle, (IP_IF_PTR)parms->ihandle); /* this one causes memory leak*/

+   error = IP_route_add_indirect(parms->network, netmask, parms->network, RTF_REDIRECT | RTF_REDIRECT_HOST, parms->locmask, (IP_IF_PTR)parms->ihandle,parms->address);

+

+   RTCSCMD_complete(parms, error);

+#else

+

+    RTCSCMD_complete(parms, RTCSERR_IP_IS_DISABLED);

+

+#endif /* RTCSCFG_ENABLE_IP4 */   

+

+} /* Endbody */

--------------------------------------------

rtcs/source/tcpip/iproute.c

--------------------------------------------

uint_32 IP_route_add_indirect

   (

      _ip_address    address,    /* Gateway address */

@@ -373,7 +373,9 @@

       _ip_address    netmask,    /* Network mask    */

       _ip_address    network,    /* Network address */

       uint_32        flag,       /* [IN] RTF_* */

-      uint_16        metric      /* [IN] the route metric [0,65535] */

+      uint_16        metric,     /* [IN] the route metric [0,65535] */

+      IP_IF_PTR      destif,     /* WMQ:Interface for outgoing packets  */

+      _ip_address    source      /* WMQ: source address to send */

    )

{ /* Body */

    IP_CFG_STRUCT_PTR                IP_cfg_ptr = RTCS_getcfg(IP);

@@ -390,6 +392,8 @@

    route->FLAGS      = flag | RTF_UP;

    route->IS_DIRECT  = NULL;

    route->METRIC     = metric;

+   route->DESTIF     = destif; //WMQ

+   route->ADDRESS    = source; //WMQ

-------------------------------------------

static boolean IP_route_test

   (

      pointer     node_data,

      pointer     data

   )

{ /* Body */

.....


   if (indirect && testdata->check_gateway) {

      do {

          if (indirect->FLAGS & RTF_UP) {

            testdata->hopdest = indirect->GATEWAY;

#if 1

            if(indirect->FLAGS & RTF_REDIRECT_HOST){

                testdata->sendit = TRUE;

                testdata->ifdest = indirect->DESTIF;

                testdata->retval = RTCS_OK;

                if (!testdata->hopsrcislocal) {

                   testdata->hopsrc = indirect->ADDRESS;

                } /* Endif */

           }

#endif

            /* Notify calling function that a gateway was found */

            testdata->check_gateway = FALSE;

            return TRUE;

          } /* Endif */

         indirect = indirect->NEXT;

      } while(indirect != route->INDIRECT);

---------------------------------------------

rtcs/source/include/ip_prv.h

---------------------------------------------


#define RTF_REDIRECT_HOST0x0008  /* created for a ICMP redirect for a host*/
0 项奖励
回复

2,979 次查看
butok
NXP Employee
NXP Employee

Hi David,

We have never tested handling of the ICMPv4 Redirect messages. So I have added the task to our backlog.

BTW: What have you used to produce the ICMPv4 redirect messages? Do you use a special/customizable switch?

Thanks,

Andrey

0 项奖励
回复

2,979 次查看
David_Wu
Contributor III

The easiest way to instrument this is to enable a Linux PC with two Ethernet(s) to act as your network gateway

On LINUX PC (acting as Router/Gateway)

Ethernet 1   (Ethernet link to real network gateway 192.168.0.1 <=> 192.168.0.100 )

ifconfig eth0 192.168.0.1 netwmask 255.255.255.0

route add default gw 192.168.0.100

Ethernet 2  ( Ethernet support two seperare class C Lan spaces 192.168.1.1/24 and 192.168.100.1/24 ) connected to a HUB or a SWITCH

ifconfig  eth1:0   192.168.1.1 netmask 255.255.255.0

route add 192.168.1.0/24 eth1

ifconfig  eth1:1   192.168.100.1 netmask 255.255.255.0

route add 192.168.100.0/24 eth1

Ensure you enable the LINUX mahine as a router.  You can do this typically through the /proc file system.

Enable IP Forwarding like such:

echo 1 >  /proc/sys/net/ipv4/ip_forward

See the link below for information on enable the sending of redirects based on interface and network load. 

http://tldp.org/HOWTO/Adv-Routing-HOWTO/lartc.kernel.obscure.html


0 项奖励
回复