how to add IP FILTER in frdnk64f120

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to add IP FILTER in frdnk64f120

797件の閲覧回数
sudhakarp
Contributor V

Hi,

     i am using KDS 2.0 and ksdk1.1.0 rtcs example code.

in ethernet to serial example code i want to add IP filter. the controller only receive(or connect) data from particular IP address only.

how to do this one. any API function available for this one.

regards,

sudhakar p

ラベル(1)
0 件の賞賛
返信
1 返信

671件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Please check your the answer in the following link

how to implement IP filtering in FRDMk64


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信