fclose on SDCard filesystemhandle hangs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

fclose on SDCard filesystemhandle hangs

2,666件の閲覧回数
TobiasBystricky
Contributor III

Hello,

if we are using the sdcard we are facing the following problem.

We are mounting the SDCard:

void SDCard::mount()

{

    static const char szOpenMode[4] = "rw";

   

    if ( (NULL != filesystem_handle) ) { return; }

    _mqx_int error_code = MFS_NO_ERROR;

   

  if (NULL == com_handle)

  {

  _mqx_uint un32Param = SPI_FLAG_FULL_DUPLEX;

  /* Open low level communication device */

  com_handle = _io_fopen(com_name, (const char *)un32Param);

  /* Install SD card device */

  if ( MQX_OK != _io_sdcard_install((char *)str(ms_szName), (SDCARD_INIT_STRUCT *)&_bsp_sdcard0_init, com_handle))

  {

  _io_puts("\n");

  _io_puts(com_name);

  _io_puts(" unable to install device.");

  }

  }

  if (NULL == sdcard_handle)

    {

  /* Open the device which MFS will be installed on */

  sdcard_handle = _io_fopen(str(ms_szName), szOpenMode);

  if (NULL == sdcard_handle) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unable to open device.");

  return;

  }

#if 1

  Tun32int un32Param = 0;

  if (IO_OK != _io_ioctl(sdcard_handle, IO_IOCTL_SET_FLAGS, (pointer)&un32Param))

  {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error setting flags ");

  return;

  }

#endif

    }

  /* Install partition manager over SD card driver */

  error_code = _io_part_mgr_install(sdcard_handle, partman_name, 0);

  if (IO_DEVICE_EXISTS == error_code)

  {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" partition manager already installed ");

  }

  else if (MFS_NO_ERROR != error_code) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error installing partition manager: ");

  _io_puts(MFS_Error_text((uint_32) error_code));

  _io_puts(" unable to open device.");

  return;

  }

  _time_delay (20);

#if 0

  if ( !isAvailable() )

  {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" no card inserted ");

  turnOff();

  return;

  }

#endif

#if 0

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" installing MFS over SD card driver...");

#endif

  /* Install MFS over SD card driver */

  error_code = _io_mfs_install(sdcard_handle, filesystem_name, (_file_size) 0);

  switch (error_code)

  {

  case MFS_NO_ERROR:

  break;

  case IO_DEVICE_EXISTS:

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" MFS already installed ");

  break;

  default:

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error initializing MFS: ");

  _io_printf("(%04x) ", error_code);

  _io_puts(MFS_Error_text((uint_32) error_code));

  return;

  }

  /* Open file system */

  filesystem_handle = _io_fopen(filesystem_name, (char)0);

  if (NULL == filesystem_handle)

  {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error opening filesystem: NULL pointer returned. ");

  return;

  }

  error_code = _io_ferror(filesystem_handle);

  if (MFS_NO_ERROR != error_code) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error opening filesystem: ");

  _io_printf("(%04x) ", error_code);

  _io_puts(MFS_Error_text((uint_32) error_code));

#if SDCARD_AUTO_FORMAT

  if (error_code == MFS_NOT_A_DOS_DISK) {

  error_code = _io_ioctl(filesystem_handle, IO_IOCTL_DEFAULT_FORMAT, NULL);

  }

  if (MFS_NO_ERROR != error_code)

  {

#endif

  return;

#if SDCARD_AUTO_FORMAT

  }

#endif

  }

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" mounted to ");

  _io_puts(filesystem_name);

}

void SDCard::unmount() {

  Tun32int error_code;

  /* Close the filesystem */

  if ((NULL != filesystem_handle)

  && (MQX_OK != _io_fclose(filesystem_handle))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error closing filesystem.");

  }

  filesystem_handle = NULL;

  /* Uninstall MFS  */

  error_code = _io_mfs_uninstall(filesystem_name);

  if ( (IO_DEVICE_DOES_NOT_EXIST != error_code) && (error_code != MFS_NO_ERROR) ) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error uninstalling filesystem ");

  _io_printf("(%04x)", error_code);

  }

  /* Uninstall partition manager  */

  error_code = _io_part_mgr_uninstall(partman_name);

  if ( (IO_DEVICE_DOES_NOT_EXIST != error_code) && (error_code != MFS_NO_ERROR) ) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error uninstalling partition manager ");

  _io_printf("(%04x)", error_code);

  }

  /* Close the SD card device */

  if ((NULL != sdcard_handle)

  && (MQX_OK != _io_fclose(sdcard_handle))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unable to close SD card device.");

  }

  sdcard_handle = NULL;

#if SDCARD_DEEP_CLEAN

  if (MQX_OK != _io_dev_uninstall((char *)str(ms_szName))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unable uninstall device.");

  }

  /* Close the ESDHC device */

  if ((NULL != com_handle) && (MQX_OK != _io_fclose(com_handle))) {

  _io_puts("\n");

  _io_puts(com_name);

  _io_puts(" unable to close ESDHC device.");

  }

  com_handle = NULL;

#endif

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unmounted.");

}

After the mounting the access to the sdcard works well.

Then we do the unmount.

void SDCard::unmount() {

  Tun32int error_code;

  /* Close the filesystem */

  if ((NULL != filesystem_handle)

  && (MQX_OK != _io_fclose(filesystem_handle))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error closing filesystem.");

  }

  filesystem_handle = NULL;

  /* Uninstall MFS  */

  error_code = _io_mfs_uninstall(filesystem_name);

  if ( (IO_DEVICE_DOES_NOT_EXIST != error_code) && (error_code != MFS_NO_ERROR) ) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error uninstalling filesystem ");

  _io_printf("(%04x)", error_code);

  }

  /* Uninstall partition manager  */

  error_code = _io_part_mgr_uninstall(partman_name);

  if ( (IO_DEVICE_DOES_NOT_EXIST != error_code) && (error_code != MFS_NO_ERROR) ) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" error uninstalling partition manager ");

  _io_printf("(%04x)", error_code);

  }

  /* Close the SD card device */

  if ((NULL != sdcard_handle)

  && (MQX_OK != _io_fclose(sdcard_handle))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unable to close SD card device.");

  }

  sdcard_handle = NULL;

#if SDCARD_DEEP_CLEAN

  if (MQX_OK != _io_dev_uninstall((char *)str(ms_szName))) {

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unable uninstall device.");

  }

  /* Close the ESDHC device */

  if ((NULL != com_handle) && (MQX_OK != _io_fclose(com_handle))) {

  _io_puts("\n");

  _io_puts(com_name);

  _io_puts(" unable to close ESDHC device.");

  }

  com_handle = NULL;

#endif

  _io_puts("\n");

  _io_puts(str(ms_szName));

  _io_puts(" unmounted.");

}

This works also well.

But after repeating the progress three time the unmount hangs in the fclose of the SDCard.

We take a deeper look inside and found out that it hangs in a sem_destroy.

Could it be a problem if different tasks mount / umount the SDCard?

Can someone help?

Thanks and regards,

Tobias

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,294件の閲覧回数
TJ
Contributor II

Hello Tobias

I was wondering if you managed to find a solution to this problem? I am experienceing a similar problem while trying to mount sd card the second time.

0 件の賞賛
返信

2,294件の閲覧回数
TobiasBystricky
Contributor III

I found out that the semaphore is not existing anymore:

2013-12-03_16h53_45.png

2013-12-03_16h55_12.png

In the semaphore overview the semaphore is not listed but a lot of semaphores with senseless content.

0 件の賞賛
返信

2,294件の閲覧回数
TobiasBystricky
Contributor III

The sem_destroy is in function _io_mfs_uninstall_internal at line 139

static int_32 _io_mfs_uninstall_internal

    (

    IO_DEVICE_STRUCT_PTR   dev_ptr  /* [IN] The device to uninstall */           

    )

{

    MFS_DRIVE_STRUCT_PTR   drive_ptr;

    int_32                 error;

    drive_ptr = (MFS_DRIVE_STRUCT_PTR)dev_ptr->DRIVER_INIT_PTR;

    if ( !drive_ptr->MFS_FILE_PTR )

    {

        error = IO_OK;

        _lwsem_destroy(&drive_ptr->SEM);

        _mfs_partition_destroy(drive_ptr->HANDLE_PARTITION);

        _mem_free(drive_ptr);

    }

    else

    {

        error = MFS_SHARING_VIOLATION;

    } 

    return error;

} 

Here line 14...

0 件の賞賛
返信