examples and debugging MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

examples and debugging MQX

跳至解决方案
1,052 次查看
Microfelix
Contributor IV

Hi, I recently started working on the K60 and precisely TWRK60-KIT. With the examplesof the K60 I have no problems. Instead if I try to run the examples of the MQX, I can not get it to compile, debug it. I do not know how to run the examples in the folder MQX.Something wrong. Can you help me or point the way to successfully run the examples?

 

thanks Maurizio

0 项奖励
回复
1 解答
864 次查看
anthony_huereca
NXP Employee
NXP Employee

I'd recommend going through the Kinetis Quick Start Demo lab, which has detailed instructions for running an MQX project and flashing/debugging it with both CodeWarrior 10 and IAR.

 

You can also look at the docs folder for two files that will also help you get up and going:

\doc\FSL_MQX_3_7_in_CW_10_1.pdf

\doc\FSL_MQX_Getting_Started.pdf

 

Hope that helps!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
865 次查看
anthony_huereca
NXP Employee
NXP Employee

I'd recommend going through the Kinetis Quick Start Demo lab, which has detailed instructions for running an MQX project and flashing/debugging it with both CodeWarrior 10 and IAR.

 

You can also look at the docs folder for two files that will also help you get up and going:

\doc\FSL_MQX_3_7_in_CW_10_1.pdf

\doc\FSL_MQX_Getting_Started.pdf

 

Hope that helps!

0 项奖励
回复
864 次查看
Microfelix
Contributor IV

Thank you.

I'm getting closer to Freescale are so many things to see

 

maurizio


0 项奖励
回复