ethernet socket issue with multiple instances

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ethernet socket issue with multiple instances

跳至解决方案
1,170 次查看
khoanguyen
Contributor I

Hi,

I'm currently using MQX 3.8.1 with Code Warrior 10.2 and the Kinetis k60 tower. I'm currently having trouble sending strings over multiple instances and was wondering if this was a timing issue.

My setup:

I have two tasks: connect_task and print_task.

the connect_task initializes RTCS and creates and connects a socket to an external server. My tower is acting as a client.

This task is successful because I sent a string confirming connection and verified that the server was able to receive it, so I know that the connection was successful and I was able to send a string over TCP/IP to a server.

Once finished it creates 5 instances of the print task and passes in 5 different strings. This is almost exactly like the mutex example provided.

the print_task is where I'm having trouble. Since I have already opened the socket, I set the same parameters and attempted to send that data the same way I did in the connect_task. I was wondering if this was a timing issue and the send was blocking.

Below is my code.

Thanks,

Khoa Nguyen

/****************************************************************************

* RYSK TECH

* RMD

* Created by: Khoa Nguyen

* Date: October 1, 2012

* Description: Demo for the CDR

****************************************************************************/

#include "main.h"

#include "mutex.h"

#if !BSPCFG_ENABLE_IO_SUBSYSTEM

#error This application requires BSPCFG_ENABLE_IO_SUBSYSTEM defined non-zero in user_config.h. Please recompile BSP with this option.

#endif

#ifndef BSP_DEFAULT_IO_CHANNEL_DEFINED

#error This application requires BSP_DEFAULT_IO_CHANNEL to be not NULL. Please set corresponding BSPCFG_ENABLE_TTYx to non-zero in user_config.h and recompile BSP with this option.

#endif

#if ! MQX_HAS_TIME_SLICE

#error This application requires MQX_HAS_TIME_SLICE defined non-zero in user_config.h. Please recompile kernel with this option.

#endif

#if ! BSPCFG_ENABLE_GPIODEV

#error This application requires BSPCFG_ENABLE_GPIODEV defined non-zero in user_config.h. Please recompile BSP with this option.

#endif

TASK_TEMPLATE_STRUCT MQX_template_list[] =

{

        /* Task Index,           Function,       Stack,  Priority,  Name,       Attributes,       Param, Time Slice */

            { IDLE_TASK,        idle_task,      2000,   7,     "idle",        MQX_AUTO_START_TASK,     0,     0 },

            { CONNECT_TASK,        connect_task,      1000,   6,     "connect",           0,                 0,     0 },

            { PRINT_TASK,       print_task,     1000,   9,     "print",        MQX_TIME_SLICE_TASK,     0,     3 },

            { 0 }

};

/*TASK*-----------------------------------------------------

*

* Task Name    : Main_task

* Comments     :

*

*END*-----------------------------------------------------*/

void idle_task(uint_32 initial_data)

{

    /*Initialize Mutex struct and hard code 4 strings*/

    MUTEX_ATTR_STRUCT mutexattr;

    char*             string1 = "1 Sensor ONE task\n";

    char*             string2 = "2 Sensor TWO task\n";

    char*             string3 = "3 Sensor THREE task\n";

    char*             string4 = "4 Sensor FOUR task\n";

   

   

    /* Initialize mutex attributes */

    if (_mutatr_init(&mutexattr) != MQX_OK) {

          printf("Initialize mutex attributes failed.\n");

          _task_block();

       } 

       /* Initialize the mutex */

    if (_mutex_init(&print_mutex, &mutexattr) != MQX_OK) {

          printf("Initialize print mutex failed.\n");

          _task_block();

       }

   

    printf("\n Welcome to the RYSK Tech RMD device \n");

  

    _task_create(0, CONNECT_TASK, 0);

       _time_delay(5000);

       /* Create the print tasks */

   _task_create(0, PRINT_TASK, (uint_32)string1);

   _task_create(0, PRINT_TASK, (uint_32)string2);

   _task_create(0, PRINT_TASK, (uint_32)string3);

   _task_create(0, PRINT_TASK, (uint_32)string4);

   _task_block();

  

}

void connect_task(uint_32 initial_data)

{

    _ip_address     ipaddr;

    uint_32         sock;

    uint_32            result;

    sockaddr_in        addr;

    char*            test = "This is a test for stream";

   

    while(1)

    {

        if (_mutex_lock(&print_mutex) != MQX_OK)

            {

                printf("Mutex lock failed.\n");

                _task_block();

            }   

    rtcs_init();

   

    addr.sin_family     = AF_INET;

    addr.sin_port        = 10000;

    addr.sin_addr.s_addr = IPADDR(192,168,3,102);

   

    sock = socket(AF_INET, SOCK_STREAM, 0);

   

    result = connect(sock, &addr, sizeof(addr));

    //_time_delay(1000);

    if(result != RTCS_OK)

        {

            printf("ERROR the socket could not CONNECT");

        }

    if(result == RTCS_OK)

    {

        printf("\nREADY TO SEND DATA!!!!!!!!!!!!!!!!!");

        printf("\nConnected to %lx, port %d",addr.sin_addr.s_addr, addr.sin_port);

    }

   

    send(sock, (void *)test, strlen(test), 0);

   

    _mutex_unlock(&print_mutex);

    _task_block();

    }

}

void print_task(uint_32 initial_data)

{

    while(1)

    {

        _ip_address     ipaddr;

        uint_32         sock;

        uint_32            result;

        sockaddr_in        addr;

        char* cBuffer;

        char tag[50];

        char             Buffer[50] ={0};

       

       

        sprintf(tag, (char *)initial_data);

       

        sprintf(Buffer, (char *)initial_data);

        cBuffer = Buffer;

       

        if (_mutex_lock(&print_mutex) != MQX_OK) {

                 printf("Mutex lock failed.\n");

                 _task_block();

              }

       

        addr.sin_family     = AF_INET;

        addr.sin_port        = 10000;

        addr.sin_addr.s_addr = IPADDR(192,168,3,102);

           

       

        send(sock, (void *)Buffer, strlen(Buffer), 0);

        _io_puts((char *)initial_data);

         _mutex_unlock(&print_mutex);

    }

}

/* EOF */


标记 (5)
0 项奖励
回复
1 解答
866 次查看
Martin_
NXP Employee
NXP Employee

Your socket handle in the print_task() is a local variable, not being initialized.
I think you should make the sock variable (socket handle) global, so that when you initialize it in the connect_task, you can refer to it from the print_task(s).

Right now, the sock variable in the print_task() is undefined value on the print_task's stack, so you can't send() via undefined socket.

在原帖中查看解决方案

0 项奖励
回复
1 回复
867 次查看
Martin_
NXP Employee
NXP Employee

Your socket handle in the print_task() is a local variable, not being initialized.
I think you should make the sock variable (socket handle) global, so that when you initialize it in the connect_task, you can refer to it from the print_task(s).

Right now, the sock variable in the print_task() is undefined value on the print_task's stack, so you can't send() via undefined socket.

0 项奖励
回复