creating and compiling FFS nandflash example in mqx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

creating and compiling FFS nandflash example in mqx

ソリューションへジャンプ
1,569件の閲覧回数
adt
Contributor III

hello all,

I am using codewarrior 10.5 and mqx 4.0.2 & TWRK60F120M. I am able to execute the nandflash example in mqx but I want to work on nandflash using MFS I have installed patch for FFS for mqx 4.0.2. But not getting how to create and compile it in mqx.

Please help me.

Thanks

ラベル(1)
0 件の賞賛
返信
1 解決策
1,223件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Check the user guide in C:\Freescale\Freescale_MQX_4_0\doc\ffs

And the demo project: C:\Freescale\Freescale_MQX_4_0\ffs\examples\mfs_nandflash

You have to build the FFS MQX library for your target and run the example.

Check the document C:\Freescale\Freescale_MQX_4_0\doc\ FSL_MQX_FFS_release_notes.pdf  "5.2. Understand MFS NAND Flash example”

Luis

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,224件の閲覧回数
LuisCasado
NXP Employee
NXP Employee

Hello,

Check the user guide in C:\Freescale\Freescale_MQX_4_0\doc\ffs

And the demo project: C:\Freescale\Freescale_MQX_4_0\ffs\examples\mfs_nandflash

You have to build the FFS MQX library for your target and run the example.

Check the document C:\Freescale\Freescale_MQX_4_0\doc\ FSL_MQX_FFS_release_notes.pdf  "5.2. Understand MFS NAND Flash example”

Luis

0 件の賞賛
返信
1,223件の閲覧回数
adt
Contributor III

Thanks for the reply. I have tested the example and its working fine.

0 件の賞賛
返信