hi,
I do all steps for install MQXOS 3.7, for test demos in TWRK40X256.
I install Updates for Codewarrior 10.1 ....
when import the bsp_twrk40x256 proyect and build proyect, send an error in line console code error looks...
**************************************************************************
Setting working directory to C:\Users\tvo\Freescale\Freescale MQX 3.7\lib\twrk40x256.cw10\bsp\Generated_Code 1 file(s) copied.
' '
'attrib' is not recognized as an internal or external command, operable program or batch file.
A subdirectory or file dbg already exists.
'attrib' is not recognized as an internal or external command, operable program or batch file. **********************************************************************************
Someone Can Help?
Solved! Go to Solution.
Hello,
Please follow the steps Gavin outlined but use most recent MQX3.8.1 release and CW10.2.
Bot have many updates/fixes/improvements that should help.
Regards,
David
Hello,
Please follow the steps Gavin outlined but use most recent MQX3.8.1 release and CW10.2.
Bot have many updates/fixes/improvements that should help.
Regards,
David
try my install steps:
1. install CW_MCU_v10.1_SE.exe
2. dont' instal MQX-3.7; If you already installed it, just un-install MQX-3.7
3. read CW_MCU_v10.1_Update_Procedure.pdf
4. Do section On-Line Mode 3.1 steps 1) to 7) in CW_MCU_v10.1_Update_Procedure.pdf
5. Do section Off Line Mode 2.1 all steps in CW_MCU_v10.1_Update_Procedure.pdf to
NOTE: select "MCU_v10.1_Compiler_Update_ColdFire_Kinetis_Qorivva_for_Windows.zip" in step 2.1-6)
6. Install "MCU v10.1 Kernel Awareness Update for Windows.zip"
according to section Off Line Mode 2.1 all steps in CW_MCU_v10.1_Update_Procedure.pdf
7. Install "CW_MCU_v10.1_Update_1.0.0.zip"
according to section Off Line Mode 2.1 all steps in CW_MCU_v10.1_Update_Procedure.pdf
****After install the Feature information indicates com.freescale.mcu is 10.1.5****
8. Install MQX-3.7
9. Run ../Setup_JLinkARM_V428c.exe to upgrade firmware for your J-Link Pro
thanks for post an solucion, but i did all the steps - install CW10.1 in not defaul path install patch (kernel,patch for MQX , update for 10.1), after this i install Freesscale MQX 3.7 I select the workspace for Freescale MQX 3.7
but the problem is before preuild the project ... an archives have some error or i dont know what is it, but apears 'attrib' is not recognized as internal or external comand this is the error, it had to be someting else in folder bat (bps.bat windows batch files)
If you are using Windows operating system on your PC, you should have "attrib" command supported.
You can check it by typing "attrib" in command line.
The attrib command is used to remove read-only flags on files in destination directory. Its for customers which have MQX installation under version control system and MQX source files are read only.
If its not your case and you have standard MQX installation, you can remove "attrib" command call from your batch file.
Has anyone found a real solution to this problem. In Windows XP with CW PA Version: 10.1.1
Build Id:111014_R1011 this appears to still be an issue. There is no problem running attrib from the command line its just when it is in a batch file invoked from the post build steps in CW. I would like to leave the attrib in for the reasons explained above.