build warning of MQX 4.2.0.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

build warning of MQX 4.2.0.2

1,006 Views
icelee
Contributor III

hello


I'm using MQX 4.2.0.2 run on FRDM-K64F.
And build MQX using KDS3.0

I import the below 4 original MQX project into KDS,
and build them in release mode as the following.

・bsp_frdmk64f
・psp_frdmk64f
・rtcs_frdmk64f
・shell_frdmk64f


build log of [bsp_frdmk64f] and [psp_frdmk64f] is well.
But [rtcs_frdmk64f] and [shell_frdmk64f] have some warning.

Details are as follows.


[rtcs_frdmk64f] build warning log:


-----------------------------------------------------------------------------------------------------------------

..\..\..\..\source\nat\dnat.c: In function 'DNAT_lookup_rule':
..\..\..\..\source\nat\dnat.c:92:75: warning: 'destination_port' may be used uninitialized in this function [-Wmaybe-uninitialized]
             if ((destination_port >= element_ptr->RULE.PUBLIC_START_PORT) &&
                                                                           ^

..\..\..\..\source\nat\dnat.c:98:71: warning: 'source_port' may be used uninitialized in this function [-Wmaybe-uninitialized]
                 (source_port >= element_ptr->RULE.PRIVATE_START_PORT) && 
                                                                       ^

..\..\..\..\source\nat\natevent.c: In function 'NAT_expire':
..\..\..\..\source\nat\natevent.c:176:48: warning: 'tmp_nat_event_ptr' may be used uninitialized in this function [-Wmaybe-uninitialized]
       tcpip_event_ptr->TIME = tmp_nat_event_ptr->TIME;
                                                ^

..\..\..\..\source\nat\natdata.c: In function 'NAT_insert':
..\..\..\..\source\nat\natdata.c:230:18: warning: 'key' may be used uninitialized in this function [-Wmaybe-uninitialized]
    IPRADIX_insert(&nat_cfg_ptr->ROOT_IN, key, 0xFFFFFFFF, nat_cfg_ptr->RADIX_IN,
                  ^

..\..\..\..\source\if\rtcsrand.c: In function 'kiss_gen_seed':
..\..\..\..\source\if\rtcsrand.c:64:17: warning: type of 'x' defaults to 'int' [enabled by default]
 static uint32_t kiss_gen_seed(x, y)
                 ^
..\..\..\..\source\if\rtcsrand.c:64:17: warning: type of 'y' defaults to 'int' [enabled by default]


..\..\..\..\source\nat\nat_apply.c: In function 'NAT_mod_ip':
..\..\..\..\source\nat\nat_apply.c:367:28: warning: unused variable 'nat_cfg_ptr' [-Wunused-variable]
    NAT_CFG_STRUCT_PTR      nat_cfg_ptr = RTCS_getcfg(NAT);
                            ^

..\..\..\..\source\nat\nat_apply.c: In function 'NAT_mod_icmp':
..\..\..\..\source\nat\nat_apply.c:649:63: warning: value computed is not used [-Wunused-value]
             mqx_htons(transport.ECHO_PTR->SEQ, nat_session_ptr->PRV_PORT);
                                                               ^

..\..\..\..\source\nat\nat_apply.c:653:63: warning: value computed is not used [-Wunused-value]
             mqx_htons(transport.ECHO_PTR->SEQ, nat_session_ptr->NAT_PORT);
                                                               ^
-----------------------------------------------------------------------------------------------------------------


[shell_frdmk64f] build warning log:

-----------------------------------------------------------------------------------------------------------------

..\..\..\..\source\rtcs\sh_ppp.c: In function 'sh_ppp_start':
\freescale_mqx_4_2\shell\source\include\sh_rtcs.h:92:19: warning: 'error' may be used uninitialized in this function [-Wmaybe-uninitialized]
        do {fprintf( _file, "%s"_format "%s", PPP_PRINT_PREFIX, ##__VA_ARGS__, "\n" );} while( 0 )
                   ^
..\..\..\..\source\rtcs\sh_ppp.c:245:24: note: 'error' was declared here
     uint32_t           error;
                        ^
-----------------------------------------------------------------------------------------------------------------

Should I ignore these warnings or fix them?

If need to fix, can someone provide an official(NXP) amendment?

Thanks.

Tags (1)
0 Kudos
Reply
4 Replies

840 Views
icelee
Contributor III

Does someone have same experience about this issue?

0 Kudos
Reply

840 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Bing:

I did a quick check of the release version with KDS 3.2 and eth_to serial demo

C:\Freescale\Freescale_MQX_4_2\rtcs\examples\eth_to_serial\build\kds\eth_to_serial_frdmk64f

Not found this issue. Could you please update your KDS to 3.2 and try it again?

pastedImage_1.png

Regards

Daniel

0 Kudos
Reply

840 Views
icelee
Contributor III

Hi Daniel


I have checked my KDS's version.
I wrote wrong version number of KDS.

Right version is below.

Kinetis Design Studio
Version: 3.2.0

That's same with your KDS.

0 Kudos
Reply

840 Views
icelee
Contributor III

Hi Daniel


Thanks for your reply.

I forget some build conditions.

Must to enable the defines below in RTCS.

#define RTCSCFG_ENABLE_NAT    1
#define RTCSCFG_ENABLE_PPP    1
#define RTCSCFG_ENABLE_VIRTUAL_ROUTES 1
#define RTCSCFG_USE_KISS_RNG   1

and warings will be appear.

I think the upper defines are disable in eth_to_serial_frdmk64f project.

Could you enable these defines in eth_to_serial_frdmk64f?

Thanks.

0 Kudos
Reply