adc_mk60.h bug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

adc_mk60.h bug

335 次查看
keithtang
Contributor IV

I am not sure if this forum is the right channel to feedback the bugs. Anyway, here you are:

 

In adc_mk60.h file (under bsp_twrk60f120m), line 50 to 52:

 

#define ADC0_SOURCE_AD4A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC0_SOURCE_AD5A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))
#define ADC0_SOURCE_AD6A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(4))

 

Obviously they should be:

 

#define ADC0_SOURCE_AD4A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(5))
#define ADC0_SOURCE_AD5A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(6))
#define ADC0_SOURCE_AD6A        (ADC_SOURCE_MODULE(1) | ADC_SOURCE_MUXSEL_A | ADC_SOURCE_CHANNEL(7))

 

 

0 项奖励
回复
0 回复数