What are the differences in MFS betwen MQX4.0 and MQX 4.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the differences in MFS betwen MQX4.0 and MQX 4.1?

ソリューションへジャンプ
1,619件の閲覧回数
pk2
Contributor III

My board has 2 K60's.  I wrote a program to have one of the K60's program the other thru the EZ_Port.  I used MQX 4.0. My program reads some configuration information from a file on a SD card and loads the K60 with data from a SREC file also stored on the SD card..  My application is based on AN44406 (KwikStik-based EzPort programmer) and uses parts of the code from the application note.  The MQX 4.0 version works fine - no problems.

I am attempting to port the code to MQX 4.1 and my application can not find the files on the SD card!!  It is the same code.  The c files were copied from the working MQX 4.0 version.  I am not sure why this is.

As a sanity check I took the section of my code that opens and reads the files on the SD card and added it to the MFS sdcard example project on a TWR-K60F120M.  This example installs the SD card with a MFS shell.     When the project is built with MQX 4.0 my code works perfectly as do the DOS commands "dir", "type", etc.  HOWEVER, when the project is built using MQX4.1 my code does not work but the DOS shell commands do work.

I stepped into the the 4.0 and 4.1 version and noted there are differences between the MQX versions.  The 4.1 files contain references to MQX_IO_OLD whatever that means.

Does anyone know of any differences between versions 4.0 and 4.1 that would/could cause the problems I am seeing?  Needless to say I am disappointed that MQX 4.1 isn't working.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,235件の閲覧回数
pk2
Contributor III

Problem solved.  One of the tasks had a stack overflow.  Increasing the stack size solved the problem

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,236件の閲覧回数
pk2
Contributor III

Problem solved.  One of the tasks had a stack overflow.  Increasing the stack size solved the problem

0 件の賞賛
返信
1,235件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Thank you for share your solution

Regards

Sol

0 件の賞賛
返信