Virtual Communication (COM) Demo - CDC device is necessary

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Virtual Communication (COM) Demo - CDC device is necessary

Jump to solution
3,420 Views
ThomNet
Contributor III

Hi

in the USB Host User's Guide, Rev. 4, Appendix C Virtual Communication (COM) Demo, under C.1 Setting Up the Demo it is mentioned: "Note: To run this demo, a CDC device is necessary"

Is there a simple CDC device to be recommended, which I can buy, to run this demo successfully?

I have a CDC device, which is a mobile telephone unit and which I have connected to my TOWER system but I'm not getting any character echoed back from it, may be because of driver incompatibility.

Therefore I'm looking for a CDC device which has been tested with the example application and works.

Thanks for helping!!

Thomas

Labels (1)
1 Solution
2,630 Views
Martin_
NXP Employee
NXP Employee

Hi Thomas,


I use Freescale's USB2SER as CDC device, tried with MQX 4.0 and TWR-K60N512 and it works.

View solution in original post

13 Replies
2,630 Views
ThomNet
Contributor III

HI Martin,

thanks for the information.

I've just ordered it.

THomas

0 Kudos
2,630 Views
ThomNet
Contributor III

Hi Martin,

I would like to ask you again for your support.

I have attached 4 photos:

1.) The terminal log of the attach process of the USB2SER to my TOWER system with 1 interface.

2.) The terminal log of the attach process of a LISA-U230 mobile phone module to my TOWER system with 5 interfaces

3.) A photo from my USB2SER EVB

4.) A photo from the LISA-U230 EVB

How can I differenciate between the 5 interfaces from MQX ? Do the interfaces have dedicated names, like tty0, tty1, tty2, tty3, tty4 and who is giving those names? If there is a name, what is the name of the USB2SER interface and where can I find it in the source code?

Thanks again for any ideas

Thomas

0 Kudos
2,629 Views
Martin_
NXP Employee
NXP Employee

I was working on similar problem, when up to 4 cdc devices could be attached to Tower usb cdc host via USB HUB.

The thing is that because we attach multiple usb devices of the same class, the usb host stack calls the same callback functions (usb_host_cdc_data_event() and usb_host_cdc_acm_event() as registered via USB_HOST_DRIVER_INFO structure) for all of them.

The assignement of file names to the attached devices is done at application level. It is in usb_host_cdc_data_event callback for the USB_INTF_EVENT case, by calling function usb_class_cdc_install_driver(data_parser, device_name)), where the device_name will be one of the file names.

So, we need to implement a solution at application level to assign "tty0:", "tty1:" ... "tty4:" file names to attached devices dynamically, and close the files when a device is detached.

My solution was based on the order of attach. I specified for my application, that the 1st attached device will be "tty0:", second "tty1:" and so forth. Then I modified the communication task in such a way that it reads/writes from/to the attached devices. When a device is detached, the corresponding file is closed and removed from a list of attached devices. I have a demo for this - modification of the default MQX demo /usb/host/examles/cdc/cdc_serial - to support 2 attached cdc devices via usb hub at one time, I think it can be extended to 5 quite easily. If you compare the attached cdc_serial.c with the MQX 4.0 default cdc_serial.c you will see differences.

2,629 Views
ThomNet
Contributor III

Hi Martin,

thanks again for your quick and very detailed reply.

I will let you know any new and positive results.

Thomas

0 Kudos
2,629 Views
ThomNet
Contributor III

2 terminal logs.jpg

Hi Martin,

I have testet your cdc_serial.c file and I have checked it with the EVBUSB2SER board and with the LISA U230 board. See the two terminal logs.

I'm wondering that with the USB2SER it opens tty0 (good guy!!) but with LISA it opens nothing. With LISA shouldn't it open at least tty0 and tty1? Do you have any idea why?

All my best

Thomas

0 Kudos
2,628 Views
Martin_
NXP Employee
NXP Employee

Hi Thomas,

I guess it is caused by the order of the events. The code I sent expects an attach event is immediately followed by an interface event, as this happens when you attach one by one device via USB hub. Your device seems to have different order of events - it goes through attach of all cdc devices, then it goes via interface events of all devices.

To modify the applicaton behavior, we can add a short code into interface event switch cases, to find index corresponding with the device that caused the interface event. Proposed cdc_serial.c is attached. Please let me know if it works.

-Martin

2,628 Views
ThomNet
Contributor III

Hi Martin,

thanks again!!

I have checked the file, you've send to me. It's the same behavior as before. I have attached the terminal log screen shot with 3 x the attach log.Terminal log with new cd_serial_2013_0218.jpg

Interesting to watch is the fact, that one control interface seems to be missing?

May be this gives a new idea?!

All my best again

Thomas

0 Kudos
2,628 Views
Martin_
NXP Employee
NXP Employee

Hi Thomas, actually, I inadvertently introduced an error in application data interface callbacks.

Hopefully this one is correct. The handling of multiple cdc data devices is at application level, it should be easy to debug.

2,627 Views
ThomNet
Contributor III

Hi Martin,

I'm still in the phase of debugging and I think, I'm getting closer.

I have another question, which probably is easy for you to answer:

Is MQX 4.0 supporting the usage of USB high speed over the TWR-SER2 board?

Thomas

0 Kudos
2,628 Views
Martin_
NXP Employee
NXP Employee

Hi Thomas,

the High speed USB (EHCI controller) is supported in twrk70f120m BSP. This BSP can work with TWR-SER2, where the high speed ULPI is connected to mini-AB receptacle.

To configure usbh/usbd library to use the ehci controller, in twrk70f120m.h we need to define:

#define USBCFG_DEFAULT_HOST_CONTROLLER    (&_bsp_usb_host_ehci0_if)

for usbh + ehci.

#define USBCFG_DEFAULT_DEVICE_CONTROLLER  (&_bsp_usb_dev_ehci0_if)

for usbd + ehci.

-Martin

0 Kudos
2,628 Views
ThomNet
Contributor III

oh I forgot, i extended MAX_CDCDEV_NUM  to 8 (#define MAX_CDCDEV_NUM  8). Therefore we get the 5 well known interfaces now. Thomas

0 Kudos
2,628 Views
ThomNet
Contributor III

Hi Martin,

thanks again.

Great, for tty0 it works (see below)! Is this also what you expected? tty1? Is this my part now to extend the source code? My LISA modul is still not responding. May be it's to early for it and it's still sleeping :-)

Speaking to ublox, they told me that only 3 tty's are responding to AT commands. May be tty0 is speaking to the non AT port? I will find out.

If you have any idea to make tty1 also working, please let me know.

All my best again

Thomas

Terminal log with new cd_serial_2013_0219.jpg

0 Kudos
2,631 Views
Martin_
NXP Employee
NXP Employee

Hi Thomas,


I use Freescale's USB2SER as CDC device, tried with MQX 4.0 and TWR-K60N512 and it works.