Viewing external RAM as lwmem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Viewing external RAM as lwmem

跳至解决方案
1,996 次查看
kecart
Contributor III

I'm using lwmem in my Kinetis project and I have external SRAM.  It is a K61 with internal SRAM at 0x1FFF0000-0x2000FFFF and External SRAM at 0xA0000000-0xA003FFFF.  Is there a way to set up MQX so the TAD can see the external memory in the "MQX Lightweight Memory Blocks" window?

0 项奖励
回复
1 解答
1,723 次查看
DavidS
NXP Employee
NXP Employee

Hi Kelly,

Not sure if this does the trick for you but I think it does.

I used the following MQX application example as my starting point.

C:\Freescale\Freescale_MQX_4_1_1_GA\mqx\examples\test

I did this on the TWR-K60F120 tower hardware.

Attached is modified linker script.  It shortened the default heap size and creates/left space for defining other lwmem pools (my example has them size 0x200).  You could define this memory anywhere as far as I can tell.

Attached it my test.c that created 4 additional lwmem pool that can be seem in the "MQX Light Memory Pools" TAD tab.

ScreenHunter_113 Feb. 27 17.01.gif

Regards,

David

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,724 次查看
DavidS
NXP Employee
NXP Employee

Hi Kelly,

Not sure if this does the trick for you but I think it does.

I used the following MQX application example as my starting point.

C:\Freescale\Freescale_MQX_4_1_1_GA\mqx\examples\test

I did this on the TWR-K60F120 tower hardware.

Attached is modified linker script.  It shortened the default heap size and creates/left space for defining other lwmem pools (my example has them size 0x200).  You could define this memory anywhere as far as I can tell.

Attached it my test.c that created 4 additional lwmem pool that can be seem in the "MQX Light Memory Pools" TAD tab.

ScreenHunter_113 Feb. 27 17.01.gif

Regards,

David

0 项奖励
回复
1,723 次查看
kecart
Contributor III

pastedImage_1.png

0 项奖励
回复
1,722 次查看
soledad
NXP Employee
NXP Employee

Hello Kelly,

Unfortunately, at this moment there is not possible to use TAD in order to see the external memory in the "MQX Lightweight Memory Blocks" window like you need. Sorry for any inconvenience that may cause.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复