Update MFS part of the MQX 3.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update MFS part of the MQX 3.7

879 Views
dor
Contributor I

Hi all

We are using MQX 3.7 with the MFS extension for sd cards. Now we would like to use sd cards greater than 4GB. Unfortunately we found out that the routine 'MFS_Get_disk_free_space' just can handle drives smaller than 4GB.

But in the current documentation of the MFS we have seen that newer versions of MFS are extended and can managing sd cards bigger than 4GB.

Is it possible to  to update the MFS part of the MQX 3.7 for example with the one of MQX 4.2?

Kind regards

Stephan

0 Kudos
Reply
1 Reply

671 Views
soledad
NXP Employee
NXP Employee

Hello Stephan,

Unfortunately there are significant changes between both versions and it is not supported to modify only the MFS part.

I suggest to migrate your project to the latest release.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply