Unable to open the file if the file name consists of more than 13 characters

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to open the file if the file name consists of more than 13 characters

900 Views
Vijayaragavan
Contributor I

Trying to migrate from MQX 3.8 to 4.1. MFS installed successfully onto SD card. creating the file onto SD and opening the same file is success(only if the file name consists of  <13 characters). if file name consists of more than 13 characters fopen returns null always...

Labels (1)
0 Kudos
Reply
1 Reply

742 Views
soledad
NXP Employee
NXP Employee

Hi Vijayaraghavan Srinivasan,


Are you using a Freescale Board?

Did you test the sdcard example that are located at the path: C:\Freescale\Freescale_MQX_4_1\mfs\examples?

The example code opens SD card device and installs MFS. It allows user to perform some basic operation with the SD card through the terminal interface for example write/copy/create/rename. It shows how to work with the driver and how to use shell commands.

Could you please try using this example?


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply