USB without MFS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB without MFS

跳至解决方案
1,121 次查看
Dougdjl
Contributor I

We are using MQX 3.6.1 with a 52259 micro. I'd like to be able to access a USB stick that contains a file loaded from a PC. Is this possible to do without the use of MFS? We're having memory issues. Even though the system has external ram we're having compiler conflicts with MFS/USB and extended memory operation. The difference between light weight memory and not.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
928 次查看
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


在原帖中查看解决方案

0 项奖励
回复
2 回复数
929 次查看
DavidS
NXP Employee
NXP Employee

The short answer is you need MFS to read a MFS formatted USB drive/stick.

Regards,

David


0 项奖励
回复
928 次查看
Monica
Senior Contributor III

Hey there Douglas!

Any updates on the project?

Sorry for the delay, we'll be shortly working on your issue if there are still memory flaws!

Regards!

Monica

0 项奖励
回复