USB stick project with the Kinetis K60N512 Tower MCU Module and MQX 3.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB stick project with the Kinetis K60N512 Tower MCU Module and MQX 3.7

1,314件の閲覧回数
ThomNet
Contributor III

Hi friends,

 

does anybody has/know an IAR workbench project where an USB stick with the TWRK60KN512 board in conjunction with MQX 3.7 and a SDCard or MicroSD- Card was realized.

 

All helpful hints and ideas are appreciated.

 

Thanks in advance

 

 

Thomas

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,051件の閲覧回数
obidon
Contributor III

I have not used 3.7 but I know mqx 3.8 has an example in program files\fresscale mqx 3.8\mfs\examples\sdcard. I have used this code to read/write to sdcard or microsd cards. There are build projects there for IAR or Codewarrior.

 

I have only used the USB as device mode connected to a PC. There is an mqx example for usb\host\examples\msd that should help you.

0 件の賞賛
返信