USB stick project with the Kinetis K60N512 Tower MCU Module and MQX 3.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB stick project with the Kinetis K60N512 Tower MCU Module and MQX 3.7

626 Views
ThomNet
Contributor III

Hi friends,

 

does anybody has/know an IAR workbench project where an USB stick with the TWRK60KN512 board in conjunction with MQX 3.7 and a SDCard or MicroSD- Card was realized.

 

All helpful hints and ideas are appreciated.

 

Thanks in advance

 

 

Thomas

Labels (1)
Tags (1)
0 Kudos
1 Reply

363 Views
obidon
Contributor III

I have not used 3.7 but I know mqx 3.8 has an example in program files\fresscale mqx 3.8\mfs\examples\sdcard. I have used this code to read/write to sdcard or microsd cards. There are build projects there for IAR or Codewarrior.

 

I have only used the USB as device mode connected to a PC. There is an mqx example for usb\host\examples\msd that should help you.

0 Kudos