USB device application in MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB device application in MQX

ソリューションへジャンプ
2,613件の閲覧回数
epl
Contributor I

Hello,

 

I am using MCF52259 DEMOKIT. I want to communicate with PC( which is a host) but I don't want to use USB device as Virtual COM port.

 

Is this idea workable?

 

Thanks in advanced!

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,303件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi,

you want to develop a device with your own communication, based on USB 2.0, but not conforming to CDC. Then you have to write your own device driver in Windows.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,303件の閲覧回数
epl
Contributor I

Hello,

 

Yes, now I use python(pyusb) in host PC to communicate with m52259, and I already have my own device driver in Windows.

But it seems that there is no gerneral usb class function in m52259 or supported usb class for my application.

 

BTW, I have done this work in m52259 with CMXUSB, but now I want to redo this work with MQX3.4.

0 件の賞賛
返信
1,303件の閲覧回数
JuroV
NXP Employee
NXP Employee

Which class you are talking about?

0 件の賞賛
返信
1,304件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hi,

you want to develop a device with your own communication, based on USB 2.0, but not conforming to CDC. Then you have to write your own device driver in Windows.

0 件の賞賛
返信