The debugger is not connected to PE device

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The debugger is not connected to PE device

ソリューションへジャンプ
1,001件の閲覧回数
davidzhou
Contributor V

Hi,

I am a newbie on freescale. Just installed MQX and Code Worrier (Ver10.6.4.) I imported Hello and Hello2 projects. Compiled and be able to debug into the program. But the debugger crashes the _SET_KERNEL_DATA inside the call _mqx( (MQX_INITIALIZATION_STRUCT_PTR) &MQX_init_struct );

The hello2_twrk60f120m is debugged as flash_debug with Target settings as TWRK60F120M_OSJTAG.

What is wrong?

Thank you,

David

0 件の賞賛
返信
1 解決策
875件の閲覧回数
davidzhou
Contributor V

This may be caused by either no license or MQX plugin was not installed. After installed MQX plugin and with activated license key, the problem runs away.

Thanks,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
876件の閲覧回数
davidzhou
Contributor V

This may be caused by either no license or MQX plugin was not installed. After installed MQX plugin and with activated license key, the problem runs away.

Thanks,

0 件の賞賛
返信