The MQX solution can be used for smartDSP(msc8251)?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The MQX solution can be used for smartDSP(msc8251)?

602件の閲覧回数
chuanzhao
Contributor I

This solution can be used in SmartDSP,such as Msc8251, to develop the ipv6?

0 件の賞賛
返信
1 返信

575件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately MQX doesn't support the MSC8251 device.:smileysad:

MQX v4.1.1 supports the below evaluation boards:

• Vybrid

• TWR-VF65GS10 Development Kit

• AutoEVB Vybrid Evaluation Board

• Kinetis

• FRDM-K64F Freescale Freedom platform

• TWR-K20D50M Development Kit

• TWR-K20D72M Development Kit

• TWR-K21D50M Development Kit

• TWR-K21F120M Development Kit

• TWR-K40X256 Development Kit

• TWR-K40D100M Development Kit

TWR-K60N512 Development Kit

• TWR-K60D100M Development Kit

• TWR-K60F120M Development Kit

• TWR-K64F120M Development Kit

• TWR-K70F120M Development Kit

• KwikStik - K40X256 based Evaluation Board

• ColdFire

• TWR-MCF51JF Development Kit

• TWR-MCF52259 Development Kit

• TWR-MCF54418 Development Kit


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信