TWRK60F120 - Working with SD and SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWRK60F120 - Working with SD and SPI

Jump to solution
1,020 Views
naftalir
Contributor III

Hi all,

does the tower k60 supports working with SD over SPI?

from the example i see that the BSP_SDCARD_GPIO_CS and BSP_SDCARD_CS_MUX_GPIO not exists anywhere in the BSP

and i cant get it work (using SPI1).

i'm working with eSDHC mode and its working ok, but need to do some tests with the SPI mode.

Thank you.

Tags (3)
0 Kudos
Reply
1 Solution
682 Views
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Looking at the schematics it looks possible.  These type of exercises are great for one and all to try.

If you try please let us know your results.

Regards,

David

View solution in original post

0 Kudos
Reply
2 Replies
682 Views
danielchai
Senior Contributor I

Hi Naftalir,

Did you get the SD card work over SPI?

I also try to SPI to handle the SD card. In the MQXIOUG.pdf, it says that it is possible to use the SPI instead of SDHC.

But when I look the code, there is no definition for the SD SPI channel. It seems there is some misleading in the document.

0 Kudos
Reply
683 Views
DavidS
NXP Employee
NXP Employee

Hi Naftalir,

Looking at the schematics it looks possible.  These type of exercises are great for one and all to try.

If you try please let us know your results.

Regards,

David

0 Kudos
Reply