Hi,
I need to use TWR-WIFI-AR4100 tower module with TWR-MCF54418. I am working with MQX 4.0.2. I added AR4100 patch to MQX. There is no example for this platform. I have to port one of available examples. I need help with it.
First I want to test my boards. I want to send some command, and check if AR4100 response is correctly, but I can't find in any manuals what exactly I should send through SPI. I want to use embedded AR4100P's stack, not host MQX's stack. I read 80-Y2300-1_A_IP_Stack_Offload_Intf_and_Porting_Gd.pdf document, but I don't fully understand how this communication works.
I would be very gratefull for any example or suggestion.