I'm trying to run the HVAC webenabled demo on a TWR K60, using MQX 3.6.2 and IAR embedded workbench. The demo stops with "Waiting for ethernet cable plug in ...".
I have connected a cable, and the ethernet port LED's are lit. TWR-SER mode is RMII, 50MHz clock routed out, and TWR-K60 set to use that clock.
Any ideas?
解決済! 解決策の投稿を見る。
Try putting the board in MII mode. The MCF52259 BSP is expecting that, not RMII. It would be the original jumper locations on the TWR-SER, which you can find in the TWR-SER user manual: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf
It seems this doesn't work:
ipcfg_get_link_active(IPCFG_default_enet_device)
If I disable this check, the demo works fine. Any tips on how to get the cable check working?
Please make sure you have the switches on serial and processor boards set according to getting started manual.
It works for me.
PetrM
Sorry, it was the security demo that stops on that cable check, but the hvac demo also doesn't correctly detect the link state.
Try putting the board in MII mode. The MCF52259 BSP is expecting that, not RMII. It would be the original jumper locations on the TWR-SER, which you can find in the TWR-SER user manual: http://cache.freescale.com/files/microcontrollers/doc/user_guide/TWRSERUM.pdf