TWR-ADCDAC Demo to run on Codewarrior w/ MQX 4.1?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-ADCDAC Demo to run on Codewarrior w/ MQX 4.1?

1,017件の閲覧回数
socci
Contributor I

Hello,

I am trying to read data from the 1859 ADC on my twr-adcdac board using Codewarrior and MQX 4.1.  I am also using the K60F120M board, but am having trouble establishing the communication between the two.  Does anyone know of a demo I can run through CW?  I know of the lab software demo, but I cannot use IAR Workbench and can't figure out how to import that lab to CW.

Thanks,

Mike

タグ(2)
0 件の賞賛
返信
1 返信

842件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Michael,

You need to create a new MQX project adding all libraries that your project needs (SHELL, MFS, RTCS etc), then copy-paste all the sources files.

The important is the source code they include and can be copy and pasted to other new projects created with the wizard.

I hope this helps, have a nice day!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信