TCP/IP Out of Memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TCP/IP Out of Memory

1,448 Views
diegoderganz
Contributor II

I'm using MQX 4.0.1 and Code Warrior 10.4

HW: M52259EVB running Int. Flash Debug

I have installed the http web server and I have a page that automaticaly update the values every 10 seconds.

In around 5-10 minutes I got "Out of Memory" in the TCP/IP Task.

Thread [ID: 0x10002] (Suspended: Signal 'Process Suspended' received. Description: Process Suspended.) 

    2 SOCK_STREAM_listen() sstream.c:526 0x0000c118 

    1 0xFF000388 (0xFF000388)()  0xff000388 

Or sometime directly "Unhandled Interrupt"

Thread [ID: 0x10002] (Suspended: Signal 'Process Suspended' received. Description: Process Suspended.)   

    2 SOCK_STREAM_listen() sstream.c:548 0x0000c1c0   

    1 0xFF000388 (0xFF000388)()  0xff000388   

What can be the problem?

Best regards,

Diego Derganz


Labels (1)
0 Kudos
Reply
0 Replies