From the MQX release notes (originally in 3.8.0 but still in release 3.8.1):
5.18 ARM MDK Keil uVision Support – Optimization in Release target MQX libraries
The code optimization level in the ARM MDK Keil uVision Release target is reduced to 0. Sporadic application crashes were observed in case any higher optimization level was used. The root cause of the issue was not known at the release date.
This seems to be a very vague and alarming release note that needs investigation. Is this an MQX issue or is this a Keil issue? Can either company step up to the plate and take ownership? Keil tech support says they know nothing of this issue. Is this issue active? Optimizations would be a very nice thing to run at some point.
Thanks,
pmt
解決済! 解決策の投稿を見る。
Hello pmt,
this issue was fixed, it was MQX issue.
The working KEIL optimizations are going to be enabled in MQX 4.0 with full functionality. If you or any other user insist on using optimization, I can provide a workaround.
Regards,
MartinK
Hello pmt,
this issue was fixed, it was MQX issue.
The working KEIL optimizations are going to be enabled in MQX 4.0 with full functionality. If you or any other user insist on using optimization, I can provide a workaround.
Regards,
MartinK
Hello,
Apparently, this MQXViewer fatal crash is still around in the latest version of microVision. I ran my session for several hours and this MQXViewer crash appeared, and the only way to get out of this crash was to terminate my microVision 4.70.0.0.
I need to troubleshoot my application, but this crash prevents me from running my application over time!
Would you please advise?
IDE-Version:
µVision V4.70.0.0
Copyright (C) 2013 ARM Ltd and ARM Germany GmbH. All rights reserved.
License Information:
Tu Nguyen
LIC=removed
Tool Version Numbers:
Toolchain: MDK-ARM Standard: 3 user Version: 4.70.0.0
Toolchain Path: C:\Keil\ARM\ARMCC\bin\
C Compiler: Armcc.Exe
Assembler: Armasm.Exe
Linker/Locator: ArmLink.Exe
Librarian: ArmAr.Exe
Hex Converter: FromElf.Exe
CPU DLL: SARMCM3.DLL V4.70.0.0
Dialog DLL: DCM.DLL
Target DLL: ULP2CM3.DLL V2.190.0.0
Dialog DLL: TCM.DLL V1.12.0.0
Message was edited by: removed details which are not supposed to be shared c0170