Setting up register URTS2 on mcf52259 for general purpose IO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up register URTS2 on mcf52259 for general purpose IO

2,536 Views
getuptime
Contributor I

I need to use the URTS2 pin on the mcf52259 as a general purpose IO pinin order  to drive  the transmit enable line of an RS 485 tranceiver.  How can one do this in MQX?

Thanks for any help.

0 Kudos
2 Replies

430 Views
JaimeR
Contributor III
I need to do the same thing, did you find out how to do it?
0 Kudos

430 Views
JuroV
NXP Employee
NXP Employee
Is there any issue with opening GPIO file having PORTUC | PORT_PIN2 and controling it?
0 Kudos