Setting up register URTS2 on mcf52259 for general purpose IO

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting up register URTS2 on mcf52259 for general purpose IO

2,416 次查看
getuptime
Contributor I

I need to use the URTS2 pin on the mcf52259 as a general purpose IO pinin order  to drive  the transmit enable line of an RS 485 tranceiver.  How can one do this in MQX?

Thanks for any help.

0 项奖励
2 回复数

310 次查看
JaimeR
Contributor III
I need to do the same thing, did you find out how to do it?
0 项奖励

310 次查看
JuroV
NXP Employee
NXP Employee
Is there any issue with opening GPIO file having PORTUC | PORT_PIN2 and controling it?
0 项奖励