Hi there,
I´ve got 2 questions regarding SPI communication under MQC with ADC´s:
1.) Is there any example for the TWR-ADCDAC-LTC Board together with K60 Board for Keil µVision?
2.) Is there any example to communicate with an Analog Devices ADC´s like the AD719x (AD7190/AD7191/AD7192) under MQX (which I can convert to µVision...)?
I think the routines under the SPI example are not helpful because the cover only memory transfers....
Thanks a lot!
解決済! 解決策の投稿を見る。
Hi Tobias,
From the top level http://www.freescale.com/tower web site you can find the product page for the TWR-ADCDAC-LTC Tower card.
This is vendor supported so the last update I see is for MQX3.7 and only using CW IDE and IAR.
Regards,
David
Oh, I also found these documents. I think Keil support is something new and Keil users are always one step behind...
Hi Tobias,
From the top level http://www.freescale.com/tower web site you can find the product page for the TWR-ADCDAC-LTC Tower card.
This is vendor supported so the last update I see is for MQX3.7 and only using CW IDE and IAR.
Regards,
David