Hello,
I've got Problems installing the S32 Design Studio IDE.
If I run the installer as admin it collects all data needed for the Installation, but aborts directly after with the errormessage "multiple instances of the installer not allowed. Exiting". If I run the installer as a regular user I get asked for admin-rights at the product-activation. When I enter my product-ID another error comes up (online as well as offline activation, screenshot below).
OS: Win7 Enterprise 64-Bit (6.1 Build 7601)
System manufacturer: Lenovo
Model: 4484Y1X
CPU: Intel Core i5 2.4 GHz
RAM: 4096 MB
Thanks in advance for your help.
已解决! 转到解答。
Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.
Worked fine after logging in as admin on my machine.
Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.
Worked fine after logging in as admin on my machine.