Hello,
When I connect my laptop to the my office network, I receive 2 DNS addresses.
However, When I use my TWR-K60D100M, with the following code , I receive only one DNS address (I assume it should be stored automatically in the DNS list, once I get an IP using the DHCP client??):
/* Get IP address from DHCP server */
result = ipcfg_bind_dhcp_wait(BSP_DEFAULT_ENET_DEVICE, FALSE, NULL); //FALSE = don't bind static IP after failure
if (result == IPCFG_OK)
{
is_successful = ipcfg_get_ip(BSP_DEFAULT_ENET_DEVICE, &ip_data);
if (is_successful)
{
// Get DNS_1 server
dns = ipcfg_get_dns_ip (BSP_DEFAULT_ENET_DEVICE, 0);
if (dns != 0)
{
// THE FIRST DNS IS VALID!!!
}
// Get DNS_2 server
dns = ipcfg_get_dns_ip (BSP_DEFAULT_ENET_DEVICE, 1); //<<=== This returns zero dns address, rather than the 2nd DNS which should have been supplied by DHCP server.
}
}
已解决! 转到解答。
Hi, after quick look at code of ipcfg_get_dns_ip function it seems, that if you use lightweight DNS resolver (which is default in MQX) only one DNS server IP is stored (in variable LWDNS_server_ipaddr) and this address is returned (zero is return value for any other DNS server index other than zero). If you want to have multiple DNS servers, than you have to use full DNS resolver by adding following configuration to file user_config.h:
#define RTCSCFG_ENABLE_LWDNS 0
#define RTCSCFG_ENABLE_DNS 1
#define RTCSCFG_ENABLE_LOOPBACK 1
Best Regards,
Karel
I have 2 DNS servers. But one return to me. No solution proposal proposed before has solved this problem.
https://community.nxp.com/message/317385?commentID=317385#comment-317385
and
https://community.nxp.com/thread/301815
The version i use is 4.2.0.2
#define RTCSCFG_ENABLE_LWDNS 0
#define RTCSCFG_ENABLE_DNS 1
#define RTCSCFG_ENABLE_LOOPBACK 1
The above suggestions did not solve the problem.
Can you help me?
Dear,
I tried to add a second and third DNS server address, but it seems not to work.
As understood in this thread, I can not use LWDNS, so I used DNS instead of LWDNS
(I use MQX3.8.1 on a K70 device)
// User_config.h :
// #define RTCSCFG_ENABLE_LWDNS 0
// #define RTCSCFG_ENABLE_DNS 1
// #define RTCSCFG_ENABLE_LOOPBACK 1
_ip_address DNS_server_ipaddr;
| DNS_server_ipaddr = inet_addr("8.8.8.8"); | // Open dns server1 | 
if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}
| DNS_server_ipaddr = inet_addr("208.67.222.222"); | // Open dns server1 | 
if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}
| DNS_server_ipaddr = inet_addr("208.67.220.220"); | // Open dns server2 | 
if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}
| printf("DNS0 | : %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,0))); | 
| printf("DNS1 | : %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,1))); | 
| printf("DNS2 | : %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,2))); | 
The result is that it seems to add the three dns servers => 3x DNS added ok
But when I print them out, I only have the last DNS IP at the first location. (so it seems the overwrite each other ???)
DNS0 : 208.67.220.200
DNS1 : 0.0.0.0
DNS2 : 0.0.0.0
Any idea's?
Thanks in advance.
Regards,
Michris
 
					
				
		
Hi Michris,
I am facing the same problem. After change the
#define RTCSCFG_ENABLE_LWDNS 0
#define RTCSCFG_ENABLE_DNS 1
#define RTCSCFG_ENABLE_LOOPBACK 1
I still only get one DNS server IP.
Did you solve it?
Thank you.
-Daniel
Hi, after quick look at code of ipcfg_get_dns_ip function it seems, that if you use lightweight DNS resolver (which is default in MQX) only one DNS server IP is stored (in variable LWDNS_server_ipaddr) and this address is returned (zero is return value for any other DNS server index other than zero). If you want to have multiple DNS servers, than you have to use full DNS resolver by adding following configuration to file user_config.h:
#define RTCSCFG_ENABLE_LWDNS 0
#define RTCSCFG_ENABLE_DNS 1
#define RTCSCFG_ENABLE_LOOPBACK 1
Best Regards,
Karel