Retrieving a second DNS server IP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Retrieving a second DNS server IP

跳至解决方案
5,205 次查看
panpwr
Contributor IV

Hello,

When I connect my laptop to the my office network, I receive 2 DNS addresses.

However, When I use my TWR-K60D100M, with the following code , I receive only one DNS address (I assume it should be stored automatically in the DNS list, once I get an IP using the DHCP client??):

/* Get IP address from DHCP server */

result = ipcfg_bind_dhcp_wait(BSP_DEFAULT_ENET_DEVICE, FALSE, NULL); //FALSE = don't bind static IP after failure

if (result == IPCFG_OK)

{

    is_successful = ipcfg_get_ip(BSP_DEFAULT_ENET_DEVICE, &ip_data);

    if (is_successful)

    {

        // Get DNS_1 server

        dns = ipcfg_get_dns_ip (BSP_DEFAULT_ENET_DEVICE, 0);

        if (dns != 0)

        {

          // THE FIRST DNS IS VALID!!!

        }

     

        // Get DNS_2 server

        dns = ipcfg_get_dns_ip (BSP_DEFAULT_ENET_DEVICE, 1); //<<=== This returns zero dns address, rather than the 2nd DNS which should  have been supplied by DHCP server.

    }

}

标签 (1)
标记 (3)
1 解答
4,493 次查看
karelm_
Contributor IV

Hi, after quick look at code of ipcfg_get_dns_ip function it seems, that if you use lightweight DNS resolver (which is default in MQX) only one DNS server IP is stored (in variable LWDNS_server_ipaddr) and this address is returned (zero is return value for any other DNS server index other than zero). If you want to have multiple DNS servers, than you have to use full DNS resolver by adding following configuration to file user_config.h:

#define RTCSCFG_ENABLE_LWDNS       0

#define RTCSCFG_ENABLE_DNS            1

#define RTCSCFG_ENABLE_LOOPBACK 1

Best Regards,

Karel

在原帖中查看解决方案

9 回复数
4,493 次查看
hfyuksel
Contributor I

I have 2 DNS servers. But one return to me. No solution proposal proposed before has solved this problem.
https://community.nxp.com/message/317385?commentID=317385#comment-317385
and
https://community.nxp.com/thread/301815
The version i use is 4.2.0.2

#define RTCSCFG_ENABLE_LWDNS 0
#define RTCSCFG_ENABLE_DNS 1
#define RTCSCFG_ENABLE_LOOPBACK 1
The above suggestions did not solve the problem.

Can you help me?

0 项奖励
回复
4,493 次查看
michris
Contributor III

Dear,

I tried to add a second and third DNS server address, but it seems not to work.

As understood in this thread, I can not use LWDNS, so I used DNS instead of LWDNS

(I use MQX3.8.1 on a K70 device)

   // User_config.h :

   // #define RTCSCFG_ENABLE_LWDNS       0

   // #define RTCSCFG_ENABLE_DNS            1

   // #define RTCSCFG_ENABLE_LOOPBACK 1

   _ip_address DNS_server_ipaddr;

   DNS_server_ipaddr = inet_addr("8.8.8.8");  // Open dns server1 

   if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}

   DNS_server_ipaddr = inet_addr("208.67.222.222");  // Open dns server1 

   if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}

   DNS_server_ipaddr = inet_addr("208.67.220.220");  // Open dns server2 

   if (ipcfg_add_dns_ip(ENET_DEVICE,DNS_server_ipaddr) == TRUE) {printf("DNS added ok");}

   printf("DNS0: %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,0)));
   printf("DNS1: %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,1)));
   printf("DNS2: %d.%d.%d.%d",IPBYTES(ipcfg_get_dns_ip(ENET_DEVICE,2)));

The result is that it seems to add the three dns servers => 3x DNS added ok

But when I print them out, I only have the last DNS IP at the first location. (so it seems the overwrite each other ???)

DNS0 : 208.67.220.200

DNS1 : 0.0.0.0

DNS2 : 0.0.0.0


Any idea's?

Thanks in advance.

Regards,

Michris





0 项奖励
回复
4,493 次查看
danielchai
Senior Contributor I

Hi Michris,

I am facing the same problem. After change the

   #define RTCSCFG_ENABLE_LWDNS       0

   #define RTCSCFG_ENABLE_DNS            1

   #define RTCSCFG_ENABLE_LOOPBACK 1

I still only get one DNS server IP.

Did you solve it?

Thank you.

-Daniel

0 项奖励
回复
4,493 次查看
michris
Contributor III

Hi Daniel,

I still have the same problem, even with the latest version of MQX.

Regards,

Michris

0 项奖励
回复
4,494 次查看
karelm_
Contributor IV

Hi, after quick look at code of ipcfg_get_dns_ip function it seems, that if you use lightweight DNS resolver (which is default in MQX) only one DNS server IP is stored (in variable LWDNS_server_ipaddr) and this address is returned (zero is return value for any other DNS server index other than zero). If you want to have multiple DNS servers, than you have to use full DNS resolver by adding following configuration to file user_config.h:

#define RTCSCFG_ENABLE_LWDNS       0

#define RTCSCFG_ENABLE_DNS            1

#define RTCSCFG_ENABLE_LOOPBACK 1

Best Regards,

Karel

4,493 次查看
panpwr
Contributor IV

I will try that, that you very much!

0 项奖励
回复
4,493 次查看
panpwr
Contributor IV

Can someone please pick this question up?

Thank you,

Lior.

0 项奖励
回复
4,493 次查看
c0170
Senior Contributor III

Hello Lior,

I am going to ask around :smileywink:

Regards,

MartinK

4,493 次查看
panpwr
Contributor IV

Thanks!

0 项奖励
回复