Hi everyone,
My device acts as a USB CDC device, my system is CW 10.2 and MQX 3.8.1; the communication channel needs a hardware flow control, I need to simulate the RTS signal to the host (and to get the simulated host CTS signal, of course!).
How can I implement this mechanism?
Is a notification event or an application event?
Many thanks
Teckna
已解决! 转到解答。
Hi Teckna,
I'm not USB expert at all (can spell it and plug mouse/keyboard/USB_Stick in).
Have you looked at the MQX example and its _README.pdf?
C:\Freescale\Freescale MQX 3.8b1\usb\device\examples\cdc\virtual_com
Page 6 has:
The USB_Notif_Callback, which is part of the callbacks initialized by
TestApp_Init is a callback function that the CDC class code uses to
signal to the user that a CDC event has happened. The four conditions
it handles are DTE activation and deactivation (for compatibility with
hardware flow control as in traditional UARTs), data received, and send
complete. The DTE conditions set and clear the start_transactions
variable which is tested in receive and send condition checks to make
sure data can be sent or received.
Hope this helps.
Regards,
David
Hi Teckna,
I'm not USB expert at all (can spell it and plug mouse/keyboard/USB_Stick in).
Have you looked at the MQX example and its _README.pdf?
C:\Freescale\Freescale MQX 3.8b1\usb\device\examples\cdc\virtual_com
Page 6 has:
The USB_Notif_Callback, which is part of the callbacks initialized by
TestApp_Init is a callback function that the CDC class code uses to
signal to the user that a CDC event has happened. The four conditions
it handles are DTE activation and deactivation (for compatibility with
hardware flow control as in traditional UARTs), data received, and send
complete. The DTE conditions set and clear the start_transactions
variable which is tested in receive and send condition checks to make
sure data can be sent or received.
Hope this helps.
Regards,
David
In our case:
PC host == DTE
K60 CDC device == DCE
In the MQX USB CDC example, USB_Notif_Callback() shows how K60 DCE can handle CDC activation/deactivation signal from DTE.
How about sending CDC activation/deactivation signal from K60 DCE to DTE ? Is there a USB device API to send activation/deactivation signal ?
Thanks,
Richard