I've changed my reference BSP configuration to disable RTCS_MINIMUM_FOOTPRINT, as I need support for multicast. Unfortunately when I do this RTCS fails to initialize at run-time with error 1136 (I'm using MQX 4.0.1).
The RTCS startup is somewhat convoluted so it's not easy to debug/troubleshoot but I gathered that this is an RTCSERR_OPEN_QUEUE_FAILED when calling RTCS_task_create(). Is there some run-time dependency I need to change? I am running the "small_ram_config" defaults.
Thanks,
PMT
已解决! 转到解答。
Please do not change the RTCS_MINIMUM_FOOTPRINT parameter (it is more for internal usage 0=MPUs, 1=MCUs).
If you need to enable a feature that is disabled, just use a configuration option that corresponds to it.
BTW:
In 4.1.0 the RTCS_MINIMUM_FOOTPRINT will disappear, to avoid this type of wrong settings.
Please do not change the RTCS_MINIMUM_FOOTPRINT parameter (it is more for internal usage 0=MPUs, 1=MCUs).
If you need to enable a feature that is disabled, just use a configuration option that corresponds to it.
BTW:
In 4.1.0 the RTCS_MINIMUM_FOOTPRINT will disappear, to avoid this type of wrong settings.
Andrey,
Good info. In user.config.h I re-enabled RTCS_MINIMUM_FOOTPRINT and added RTCSCFG_ENABLE_IGMP, and this seemed to take care of the issue.
My board is a derivation from the original K60 tower BSP with lots more memory. Are you saying even then I should leave RTCS_MINIMUM_FOOTPRINT enabled, and simply pick the services I need?
Thanks,
PMT