RTCS_FD_CLR() function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTCS_FD_CLR() function

跳至解决方案
2,649 次查看
emanueletrapani
Contributor III

hi, i migrated from mqx 4.1 to mqx4.2, i use CW 10.6 and frmk64f.

in my application i used the RTCS_selectset() functionand it work properly; i read in the documentation of the rtcs that is recommended the use of the select() function. i seen the example and i try to use it with some changes. everything is ok till i use the RTCS_FD_CLR() function.

my application comunicates with my pc so i use a set of socket and i must check the activity of those sockets. i'm inside a while cycle and sometimes i need to add or remove a socket from the set. adding socket happens correctly but when i try to remove the socket from the set i have some problems:

-if i use the RTCS_FD_CLR() function, when the cycle come again on the select() function it return a error 0x1716 that in rtcs_err.h is RTCSERR_SOCK_EBADF. I seen that is a error returned when the select() function check if the socket is in the socket set.

if i do not use the RTCS_FD_CLR(), the select() function return the same error.

so my question is: there is a way to use correctly the RTCS_FD_CLR() function? or there is a way to know if i use correctly this function?

now i'm trying to clear all the set and i add again all the socket i need.

a very semplified version of my cycle is:

while(1){

     err=select(active_socket_number,&sock_set,NULL,NULL, 0);

     ...

     else{

          if(RTCS_FD_ISSET(serv_sock, &sock_set)){

               accept(...);

               RTCS_FD_SET(sock,&sock_set);

               active_socket_number++;

               ...

          } else {

               rx_count=recv(sock,buf,buf_size);

               if (rx_count==RTCS_ERROR) {

                    RTCS_FD_CLR(sock,&sock_set)

                    closesock(sock);

                    active_socket_number--;

                    ...

               }

          ...

          }

     ...

}

ps: i use multiple select() function of different set of sockets in different task. But those different set may contain the same socket. can this be the problem?

0 项奖励
回复
1 解答
2,494 次查看
Martin_
NXP Employee
NXP Employee

select() changes the sock_set when it returns. Therefore you must to re-fill sock_set before select() each time it is called - in every while cycle.

while(1)

{

    RTCS_FD_ZERO(&sock_set);

    RTCS_FD_SET(sock1, &sock_set);

    RTCS_FD_SET(sock2, &sock_set);

    select(...)

 

}

You can have two sets. In one set you could keep the active sockets (add a connected client, remove disconnect client). And then before select() you just copy this set to another which is given to select():

while(1)

{

    memcpy(&sock_set, &sock_set_init, sizeof(rtcs_fd_set));  

    select(..&sock_set.)

    RTCS_FD_SET(client_sock, &sock_set_init); /* add established socket */

    RTCS_FD_CLEAR(client_sock, sock_set_init);  /* remove closed socket */

}

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,495 次查看
Martin_
NXP Employee
NXP Employee

select() changes the sock_set when it returns. Therefore you must to re-fill sock_set before select() each time it is called - in every while cycle.

while(1)

{

    RTCS_FD_ZERO(&sock_set);

    RTCS_FD_SET(sock1, &sock_set);

    RTCS_FD_SET(sock2, &sock_set);

    select(...)

 

}

You can have two sets. In one set you could keep the active sockets (add a connected client, remove disconnect client). And then before select() you just copy this set to another which is given to select():

while(1)

{

    memcpy(&sock_set, &sock_set_init, sizeof(rtcs_fd_set));  

    select(..&sock_set.)

    RTCS_FD_SET(client_sock, &sock_set_init); /* add established socket */

    RTCS_FD_CLEAR(client_sock, sock_set_init);  /* remove closed socket */

}

0 项奖励
回复
2,494 次查看
emanueletrapani
Contributor III

thank you martin!

i resolved using one select() for one socket! but your solution is better! i keep in mind for the next time!

have a nice day!

0 项奖励
回复