I'm using MQX 3.8, IAR 6.30, and a K60 TWR-K60N512 and TWRSER. I'm trying to run the ipc_udp RTCS example but the call to RTCS_Create returns an error and causes the program to enter the idle task loop rather than start sending messages. Debugging shows that the value of error after the error = RTCS_Create(); call is 4406 (which may be the decimal representation of an error code 0x1136?). I haven't been able to find reference to either error code in the code or documentation.
This is the provided MQX code for cpu1 of the ipc_udp example and hasn't been modified except for updating \config\twrk60n512\user_config.h from #include "small_ram_config.h" to #include "maximum_config.h" since small_ram_config had MQX_USE_IPC defined as 0. I have rebuilt the MQX libraries since modifying user_config.
I don't know why this provided example code isn't working and have been stuck on this for a while now. Has anyone else encountered this or does anyone have any ideas?
Thanks,
Jeff
Hi, i was with the same problem in a KSDK Processor expert project and I add the next configuration:
Select menu Project > Properties
Select C/C++ Build > Settings
Select Cross ARM C++ Linker > Libraries
Add new Libraries (-I)...
ksdk_platform_mqx
_rtcs
_mqx
_mqx_stdlib
Add new Library search path (-L)...
"${ProjDirPath}/Project_Settings/Linker_Files"
"${KSDK_PATH}/lib/ksdk_mqx_lib/kds/K64F12/Debug"
"${KSDK_PATH}/rtos/mqx/lib/frdmk64f.kds/debug/mqx"
"${KSDK_PATH}/rtos/mqx/lib/frdmk64f.kds/debug/mqx_stdlib"
"${KSDK_PATH}/middleware/tcpip/rtcs\lib/frdmk64f.kds/debug/rtcs"
------------------------------------------------------------------------------------------------------------
------------------------------------------------------------------------------------------------------------
------------------------------------------------------------------------------------------------------------
For project without processor expert:
Select Cross ARM C++ Linker > General
Script files (-T)
"C:\Freescale\KSDK_1.2.0\platform\devices\MK64F12\linker\gcc\MK64FN1M0xxx12_flash.ld"
Select Cross ARM C++ Linker > Libraries
Add new Libraries (-I)...
ksdk_platform_mqx
_rtcs
_nshell
_mqx
_mqx_stdlib
gcc
c
supc++
m
nosys
Library search path (-L)..
C:\Freescale\KSDK_1.2.0/lib/ksdk_mqx_lib/kds/K64F12/debug
C:\Freescale\KSDK_1.2.0\middleware\tcpip\rtcs\lib\frdmk64f.kds\debug\rtcs
C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\nshell
C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx
C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx_stdlib
Select Cross ARM C++ Linker > Micellaneus
C:\Freescale\KSDK_1.2.0\lib\ksdk_mqx_lib\kds\K64F12\debug\libksdk_platform_mqx.a
"C:\Freescale\KSDK_1.2.0\middleware\tcpip\rtcs\lib\frdmk64f.kds\debug\rtcs\lib_rtcs.a"
C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx_stdlib\lib_mqx_stdlib.a
C:\Freescale\KSDK_1.2.0\rtos\mqx\lib\frdmk64f.kds\debug\mqx\lib_mqx.a
Hi Jeff,
Before calling RTCS_Create (), try to modify and test the value of the following variables:
_RTCSPCB_init
_RTCSPCB_grow
_RTCSPCB_max
_RTCS_msgpool_init
_RTCS_msgpool_grow
_RTCS_msgpool_max
_RTCS_socket_part_init
_RTCS_socket_part_grow
_RTCS_socket_part_max
You can find more information about these settings in the document MQXRTCSUG.pdf.
Good luck
![]()
Thanks for the reply Tgomes. I checked the values of those variables just before RTCS_create() was called and tried modifying some of their values but still got the same error. Then I tried changing _RTCSQUEUE_base just to give it a shot. I changed it from 16 to 8 and it worked. I'm not sure exactly what effect this has but all I needed was _RTCSQUEUE_base = 8; before the RTCS_create call. Thanks for help!